LPC54606 firmware.bin filesize

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54606 firmware.bin filesize

1,640 Views
vijo
Contributor III

Hi,

when booting to USB Mass Storage Device, the size of the firmware.bin file is 516K = 512K + 4K

The size of the internal CPU flash is 512K.

Where does the 4K come from ?

Regards

Viggo

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,443 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Viggo,

Please refer the following community post: https://community.nxp.com/message/1023684 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply