LPC54606 firmware.bin filesize

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54606 firmware.bin filesize

1,151 次查看
vijo
Contributor III

Hi,

when booting to USB Mass Storage Device, the size of the firmware.bin file is 516K = 512K + 4K

The size of the internal CPU flash is 512K.

Where does the 4K come from ?

Regards

Viggo

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

954 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Viggo,

Please refer the following community post: https://community.nxp.com/message/1023684 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复