LPC54606 USB0 HOST not detecting keyboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54606 USB0 HOST not detecting keyboard

ソリューションへジャンプ
1,733件の閲覧回数
nagarajan
Contributor II

 

We have made custom board with LPC54606 micro(revision 18151A) with core clock of 180Mhz.

I am testing host on USB0 interface for past two week.

USB PLL is setup with 48Mhz and verified via CLKOUT. USB registers details below:

nagarajan_2-1606967800438.png

 

All OHCI registers are setup with values:

nagarajan_1-1606967368582.png

The HCFMREMAINING and HCFMNUMBER are changing. RHSC interrupt is not detecting on keyboard insertion. But pull up is happing on DM pin. There is no activity on DP and DM pins.

Only SF interrupt is detecting.

VBUS output and overcurrent status input is OK. USB_ID pin with low or High also checked.

Please anyboby give some information or pointer for probable causes.

 

V.Nagarajan

0 件の賞賛
返信
1 解決策
1,710件の閲覧回数
nagarajan
Contributor II

I have found a reason for USB keyboard not detecting.

USB0 HOST Function also needs a USB0_VBUS signal.

But see the user manual

 

nagarajan_0-1607052415414.png

I lost two weeks of my debugging time.

Please NXP team review the data sheet and user manual for LPC546XX.

I am sharing this so that others trying this can benefit.

Now i am going to check USB1 HS as host, surprises can be there!?

 

V.Nagarajan

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,711件の閲覧回数
nagarajan
Contributor II

I have found a reason for USB keyboard not detecting.

USB0 HOST Function also needs a USB0_VBUS signal.

But see the user manual

 

nagarajan_0-1607052415414.png

I lost two weeks of my debugging time.

Please NXP team review the data sheet and user manual for LPC546XX.

I am sharing this so that others trying this can benefit.

Now i am going to check USB1 HS as host, surprises can be there!?

 

V.Nagarajan

 

 

 

0 件の賞賛
返信