LPC54606 : I/O state in IAP (Reinvoke ISP)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54606 : I/O state in IAP (Reinvoke ISP)

2,516 次查看
karimboallal
Contributor I

Hello,

I'm working with a LPC54606J512BD208 and I'm using the IAP command "Reinvoke ISP" to update the firmware.
When I set some outputs to '0' state, the state is maintening during isp mode while with somes other output, the state change to default state (input pull-up).
For example the state is maintening with PIO4_15, PIO2_22, PIO2_23, PIO3_29 but not with PIO1_19, PIO1_20, PIO1_16, PIO0_19.

I sense that it's depend of the port number... But nothing is specified either into datasheet nor into user manual except that default state of all pins is input pull-up (except I2C open drain pins).

Someone know what is the criteria to select a pin with its state is maintening during isp mode?

Best Regards,

Karim.

标签 (2)
0 项奖励
回复
3 回复数

2,377 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Karim BOALLAL,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Whether you want the state of all pin stick to same when the MCU enter the ISP mode via the Reinvoke ISP command.
If yes, in opinion, I'm afraid it's almost impossible because we don't know the exactly code in the ROM bootloader, it may initialize some pins during the code.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,377 次查看
karimboallal
Contributor I

Hi jeremyzhou ,

Thank you for your prompt response.

I don't want the state of all pin stick to same, but I want to know which pins are not intialized (not change) when the MCU enter the ISP mode.

I don't have custom bootloader so it 's the "original" bootloader.

Is it possible to tell me which pins are not initialized during bootloader?

Best Regards,

Karim.

 

0 项奖励
回复

2,377 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Hi jeremyzhou ,

Thanks for your reply.
To be honest, it's not 100% sure.
In my opinion, the ROM bootloader will initialize the pins which are determined by the selected ISP type, in another word, the ROM bootloader will initialize the pins of the related peripheral after entering ISP mode.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复