LPC54605xx DMA to SPI hardware transfer using linked list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54605xx DMA to SPI hardware transfer using linked list

1,156件の閲覧回数
carson_cummins
Contributor I

Hi,

I'm a developer attempting to implement a linked list transfer via the DMA/DMA SPI SDK provided by NXP. Are there any examples of linked list transfers that NXP would be willing to provide?

Thanks!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,068件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Carson Cummins

Sorry we don't have DMA linked list example so far.

While we have basic DMA and SPI_DMA demo under SDK:

pastedImage_9.png

pastedImage_10.png

you can download SDK from:  https://mcuxpresso.nxp.com/en/select 

So you can refer to linked list part in Refer Manual to config based on these demo.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信