LPC54605 doesn't start SW execution after power recycling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54605 doesn't start SW execution after power recycling

3,614件の閲覧回数
Elmar
Contributor II

Hi,

I switched to LPC54605J512 MCU because of its performance.

However, the program doesn't start automatically after power recycling. I need to reprogram the MCU to make the SW start execution.

The RST pin is linked to VCC and I use Keil as a development environment.

Below you will find the programming jlink configuration screenshots.

Thanks for your feedback and help.

BR.

Elmar_0-1690185453243.png

Elmar_1-1690185468522.png

 

 

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,592件の閲覧回数
Elmar
Contributor II

Thanks, XiangJun for your reply

What a stupid design by NXP!, usually default value makes MCU boot from internal memory. 

As I already designed and manufactured my PCBA, how can I make it to boot from internal flash? Can I set internal pullup resistors from Config Tool?

0 件の賞賛
返信

3,571件の閲覧回数
carstengroen
Senior Contributor II

The only thing "stupid" here is not reading the datasheet and users manual when designing stuff.

Did you also not read that it needs 3.3V, did you apply 12V ? I guess not.
Time to do a respin...

Its written pretty clearly.....

carstengroen_0-1690206806494.png

 

0 件の賞賛
返信

3,585件の閲覧回数
frank_m
Senior Contributor III

By reading the user manual beforehand, and testing the code sufficiently.
The "stupidity" is here not on NXP's side.

I never came across a commercial design in my career were the final version was identical to the first prototype.

3,601件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you want to LPC54605 to run from internal flash after power on, you have to set the three pins PIO0_4, PIO0_5 and PIO0_6 pins high logic by connecting a pull-up resistor on the three PIO0_4, PIO0_5 and PIO0_6 pins so that the chip will fetch/execute code from internal flash after power-on.

Hope it is helpful

BR

XiangJun Rong

xiangjun_rong_0-1690194642369.png

 

3,539件の閲覧回数
Elmar
Contributor II

Dear XiangJun 

Is there another "surprise" point such as ISP configuration that I need to know before redesigning my circuit using LPC54605? 

And another question about the programming, when I used LPC845, Normal reset was enough to make the chip run the main program after flashing, but I need absolutely select Core Reset for LPC54605. Any feedback? 

Also, when I use Segger RTT viewer connected, I can't flash the chip, however, it was possible when I used LPC845. 

Thanks again for your valuable feedback. 

Elmar

0 件の賞賛
返信

3,508件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to section 13.3 Connecting power, clocks, and debug functions in data sheet of LPC546xx, which can be downloaded from the website:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

BTW, pls refer to the section 6.2.1 Termination of unused pins in the data sheet.

Hope it can help you

BR

Xiangjun Rong

 

 

 

xiangjun_rong_0-1690338198360.png

 

0 件の賞賛
返信