LPC546 MCAN not sending data continuously.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC546 MCAN not sending data continuously.

2,180 次查看
emb02
Contributor V

I am trying to interface MCAN and want to send data continuously but when I disconnect CAN H or CAN L line it will sets error and giving kStatus_MCAN_TxBusy status. it is not giving idle status when i connect line again. please help me to continuous communication between CAN. I am initiating can using config tools.

标签 (2)
标记 (3)
0 项奖励
回复
3 回复数

2,161 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

What do you mean "when I disconnect CAN H or CAN L line"? do you means that you disconnect both the CAN H or CAN L line between transmitter and receiver nodes?

BR

XiangJun Rong

0 项奖励
回复

2,156 次查看
emb02
Contributor V
yes I am disconnecting CAN H, CAN L .
0 项奖励
回复

2,152 次查看
frank_m
Senior Contributor III

Educate yourself about the meaning of transmit / receive errors, error passive state, and bus-off state, which are intrinsic part of the CAN specification.

0 项奖励
回复