LPC541xx performance: Different DMIPS but similar coremark?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC541xx performance: Different DMIPS but similar coremark?

6,869 Views
kembed
Contributor II
Hi, 

I was looking at LPC54102 and LPC54114 MCUs (both dual core MCUs M4F/M0+ but different flash and RAM) when I found that their DMIPS is very different. Here is the link LPC541XX|NXP .

LPC54102 - 220 DMIPS
LPC54114 - 125 DMIPS

Even though they have different DMIPS, their coremark performance is very similar, ~2.6 iterations/MHz for both MCUs when M4F is active. (I have also attached pics from datasheet)

Could someone please explain why these MCUs have so different DMIPS when both MCUs have exact same processor cores? Is this a mistake on the website or there are some other factors that affect MCU performance this much?

Thanks,
Labels (2)
4 Replies

6,438 Views
converse
Senior Contributor V

Looks like a mistake to me.

According to the ARM documents here: ARM Information Center, the Cortex-M4 has a rating of 1.25 DMIPS/MHz with 0 wait-state memory (for comparison, the Cortex-M3 is 1.24 DMIPS/Mhz). So, at 100MHz, the DMIPS is 125 - and that will be the maximum possible. So the 220 number looks bogus (this would imply a clock frequency of 176MHz).

6,438 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Con Verse,

Thank you for your interest in NXP Semiconductors products and the opportunity to serve you.

DMIPS figures is susceptible to many other factors, besides the true performance of the CPU. Often, the variation in performance is due to the efficiency of the C compiler.

There are the DMIPS figures with the compiler optimization.

Regarding to Cortex-M3, they are 1.25/1.50/1.89 DMIPS/MHz.

Regarding to Cortex-M4, they are 1.25/1.52/1.91 DMIPS/MHz (without FPU) and 1.27/1.55/1.95 DMIPS/MHz (with FPU).

And regarding to the 220 DMIPS, only some dual core MCU can be able to get.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,438 Views
kembed
Contributor II

Hi jeremyzhou, 

Thanks for the reply. Could you please explain in little more detail how the DMIPS number were obtained for LPC54102 (220 DMIPS) and LPC54114 (125 DMIPS) MCUs (both dual core M4F/M0+) that are on the website LPC541XX|NXP ?

Like, were both the cores running or it was just Cortex M4? Did you use the same optimized C compiler for both? If not, is there is a way to get the same performance out of LPC54114 by optimizing the C compiler the same way it was optimized for LPC54102 ? 

I am just trying to compare the performance of LPC54114 and LPC54102 MCUs but huge difference in DMIPS number is making it confusing. 

Thanks,

0 Kudos
Reply

6,438 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Kam Saini

Thanks for your reply.

Actually, I've also had none further information about the DMIPS of the LPC54102 and LPC54114.

According to the DMIPS figures, we can recognize the design purpose of these two MCU is not same definitely.

And I've also contacted with the AE team, and their reply is consist with my guess.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply