LPC5411x battery backup and maximum operating frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5411x battery backup and maximum operating frequency

1,317件の閲覧回数
miloslav
Contributor I

Is there any recommended schematic to backup RTC of the LPC5411x by coin cell?

I am a bit confused about maximum frequency too. Datasheet says maximum frequency is 150 MHz, however User manual says up to 100 MHz. Which number is valid.

0 件の賞賛
返信
1 返信

1,303件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi miloslav 

LPC5411x RTC and its oscillator continue running in all reduced power modes as long as power is supplied to the device.

RTC module runs from device power pins. There is no dedicate power supply pin to LPC5411x RTC module.

LPC5411x both cores  maximum frequency is 150 MHz.

Have a nice day,

Jun Zhang

 

 

0 件の賞賛
返信