LPC54114 audio line-in for sensory commands instead of mic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54114 audio line-in for sensory commands instead of mic

1,234件の閲覧回数
david_hille
Contributor I

For the LPC54114 audio and voice recognition kit is it possible to use the line-in audio port instead of the mic to send the Sensory keyword and commands?  If so, how do I enable this?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,148件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David

NXP supports questions related to the MCU hardware and drivers (DMIC interface and Hardware VAD etc.) via the internal LPC community forum. Questions about voice triggering performance and integration that is not related to the MCU hardware should be referred to Sensory.

For more, see https://community.nxp.com/docs/DOC-332211 

Have a nice day,

Jun Zhang

0 件の賞賛
返信

1,148件の閲覧回数
david_hille
Contributor I

OK, thank you for the quick response on this.

David Hille | Owner / CEO

Moderno Technologies, Inc.

(360) 624-5538

ModernoTechnologies.com

0 件の賞賛
返信

1,148件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信