LPC54113 Controller RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54113 Controller RAM

Jump to solution
1,825 Views
PK_1114
Contributor II

Dear Sir,

 

In the LPC54113 Controller RAM Area is erased by the software, Watchdog Reset time.

 

Thank You,

B Pavan Kumar

0 Kudos
Reply
1 Solution
1,812 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that there is not erasing concept for SRAM,you can write any data at any time to an address of SRAM. In  general, after reset, the data in SRAM is random, even if the data in SRAM are all zero, you can not take it for granted.

Hope it can help you

BR

XiangJun Rong

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,813 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that there is not erasing concept for SRAM,you can write any data at any time to an address of SRAM. In  general, after reset, the data in SRAM is random, even if the data in SRAM are all zero, you can not take it for granted.

Hope it can help you

BR

XiangJun Rong

 

 

0 Kudos
Reply
1,806 Views
frank_m
Senior Contributor III

To expand on that, SRAM is usually initialized in the startup code.
Most regions are cleared (to zero), others are initialized with constant data from Flash, according to the linker script settings.

If one want to change this behavior, this would be the place to implement it, i.e. the startup code in connection with the linker script and section definitions.

0 Kudos
Reply