LPC5410x FIFO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5410x FIFO

4,055件の閲覧回数
rogerlittlewood
Contributor I

Is it correct that the max FIFO size in the System FIFO for a UART is 16 bytes?

If this is so, I don't get why the system FIFO thing exists, why not just put the buffer in the UART like everyone else, or am I missing something?
Roger

0 件の賞賛
返信
1 返信

3,106件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Roger,

Yes, you're right.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信