LPC5410x FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5410x FIFO

4,035 Views
rogerlittlewood
Contributor I

Is it correct that the max FIFO size in the System FIFO for a UART is 16 bytes?

If this is so, I don't get why the system FIFO thing exists, why not just put the buffer in the UART like everyone else, or am I missing something?
Roger

0 Kudos
Reply
1 Reply

3,086 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Roger,

Yes, you're right.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply