LPC5410x Errata : POWER_API.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC5410x Errata : POWER_API.1

1,397 次查看
BTaylor
Contributor III

There is a section in the LPC5410x Errata Sheet (ES_LPC5410x) entitled: "POWER_API.1: The set-voltage API ROM call does not configure the internal regulator correctly for the desired operating frequency"

The stated workaround is the use the power_lib library in LPCOpen v3.xx when setting voltage for a given frequency. 

Based on NXP guidance, we are using the MCUxpresso SDK instead of the LPCOpen SDK for our LPC54102 project. 

Is the POWER_SetVoltageForFreq() function in the MCUXpresso SDK safe to use? In other words, is it implemented such that it avoids the issue described in the errata sheet?

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,373 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that it is safe to use the void POWER_SetVoltageForFreq(uint32_t freq); which is defined in the fsl_power.h, the api function can set up LDO output voltage based on core frequency.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复