LPC5410x : Clock Cross-Check

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC5410x : Clock Cross-Check

1,217 次查看
BTaylor
Contributor III

Is there a quick (and relatively easy) way using the LPCopen libraries to cross-check the rate of an external clock with that of an internal clock (e.g. IR or RTC)? This would be part of a power-up self-test to ensure that the rate of the external clock is within tolerance (or at least that it is relatively consistent with the internal clock(s)).

0 项奖励
回复
1 回复

1,205 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

There is a way to monitor some clocks by using CLKOUT pin. Using this feature you can select and observe certain clocks through an external pin.

FelipeGarcia_0-1612912119348.pngFelipeGarcia_0-1612912119348.png

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复