LPC54102 power rail leakage?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54102 power rail leakage?

1,711 次查看
StephenYeh
Contributor III

Hi,

Is it possible that power rail design

@ VDDA:3.3V / VDD:1.8V / VREFN: 0V / VREFP:2.5V ?

We got the issue that VDD will leakage to 2.3V.

 

StephenYeh_0-1660053260817.png

 

 

0 项奖励
回复
3 回复数

1,708 次查看
StephenYeh
Contributor III

Hi,

I check the spec.(the leakage will from VIA design(it will refer. VDD) right?

StephenYeh_0-1660092919193.png

 

 

0 项奖励
回复

1,667 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi StephenYeh 

This issue is linked with a internal ticket. I will keep you informed if any update.

For now, I suggest you setting VDDA equal to VDD.

Thanks,

Jun Zhang

0 项奖励
回复

1,612 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @StephenYeh 

In the limiting table, the analog input voltage should say VDDA instead of VDD. When the ADC is used, the signal levels signal levels on analog input pins must not be above the level of VDDA at any time.

Hope this helps,

Jun Zhang

0 项奖励
回复