LPC54102 power rail leakage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54102 power rail leakage?

1,708件の閲覧回数
StephenYeh
Contributor III

Hi,

Is it possible that power rail design

@ VDDA:3.3V / VDD:1.8V / VREFN: 0V / VREFP:2.5V ?

We got the issue that VDD will leakage to 2.3V.

 

StephenYeh_0-1660053260817.png

 

 

0 件の賞賛
返信
3 返答(返信)

1,705件の閲覧回数
StephenYeh
Contributor III

Hi,

I check the spec.(the leakage will from VIA design(it will refer. VDD) right?

StephenYeh_0-1660092919193.png

 

 

0 件の賞賛
返信

1,664件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi StephenYeh 

This issue is linked with a internal ticket. I will keep you informed if any update.

For now, I suggest you setting VDDA equal to VDD.

Thanks,

Jun Zhang

0 件の賞賛
返信

1,609件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @StephenYeh 

In the limiting table, the analog input voltage should say VDDA instead of VDD. When the ADC is used, the signal levels signal levels on analog input pins must not be above the level of VDDA at any time.

Hope this helps,

Jun Zhang

0 件の賞賛
返信