LPC54102 cutom bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54102 cutom bootloader

3,232 次查看
eu_mtaverna
Contributor III

Hi All,

My goal is build a bootloader in order to launch and if needed upgrade, my application.

I'm working witu MCUxpresso and LPC54102 microcontroller.

I have already build the bootloader project named SBL.c, thi code is a single core code mapped in the first sector of the LPC Flash memory (Location 0x0, size 0x8000).

I have build also a simple application that toggle a led by one of the GPIO port just to debug the bootloader. This second application is mapped on the second sector of LPC Flash memory (Location 0x8000, size 0x8000).

When I launch the SBL.c by debugger the it goes on a fault condition when it is calling the second application .... Attached a part of SBL.c and a Debugger error.

I have also tryed to leave the SBL.c running without the debugger but it seems not working.

 

//SBL.c

//Define my Application Address
#define APPLICATION_ADDRESS 0x00008020
typedef void(*pFunction)(void);
pFunction appEntry;
uint32_t appStack;

//Disabling interrupts, before changing interrupt vectors
__disable_irq();

//Get the application stack pointer
appStack=(uint32_t)*((__IO uint32_t*)APPLICATION_ADDRESS);

//Get the application entry point
appEntry=(pFunction)(__IO uint32_t*)(APPLICATION_ADDRESS+4);

// Set vector table offset
SCB->VTOR = APPLICATION_ADDRESS;

//Enable interrupts before jumping to application
__enable_irq();

//Set application stack pointer
__set_MSP(appStack);

appEntry();        //Errors appear when call this function

 

DebuggerError.PNG

Thanks in advance.

 

0 项奖励
回复
4 回复数

3,218 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @eu_mtaverna,

Could you please try declaring the appEntry(); as follows?

static void(*appEntry)(void)=0;
appEntry=(void(*)())(APPLICATION_ADDRESS+4);
appEntry();

Also, could you please read the following application note? https://www.nxp.com/docs/en/application-note/AN11610.zip. It might be useful.

Best regards, Raul.

 

0 项奖励
回复

3,206 次查看
eu_mtaverna
Contributor III

Hi, Thanks a lot for replay, the issue was about the systick interrupts that I haven't disabled....

Now the bootloader works and can start correctly a single core application.

Now a new issue appears with a dual core application: when the bootloader lounch a dual core application only the Master core seems to starts. The Slave core seems to loop in boot condition.... Have you any Idea about??

0 项奖励
回复

3,203 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @eu_mtaverna,

Could you please take a look to the following application notes related with the dual core applications?

Regards, Raul.

0 项奖励
回复

3,180 次查看
eu_mtaverna
Contributor III

Hi RaulRomero, I have take a look to the application notes as you seggest, but I have not fix.. The issue seems in the Chip_CPU_CM0Boot(uint32_t *coentry, uint32_t *costackptr) function.

When the above function clears the Slave Reset an HardFault (HFSR) appears. At first I thought about a Debugger problem, but also without Debugger the CM0 Slave don't starts correctly.

Do you have suggestion about in order to investigate?

Thanks

 

0 项奖励
回复