Brownout detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Brownout detection

1,994件の閲覧回数
Pranavmv012
Contributor I

Hello, 

I am looking for brown out detection examples for LPC 1758 mcu, it is not clear how this should be enabled and how the interrupt is triggered. 

Is there any standard library for this. Please provide a coding example. 

Thanks in advance. 

 

0 件の賞賛
返信
2 返答(返信)

1,947件の閲覧回数
Pranavmv012
Contributor I

Is it possible to set the voltage level at which the interrupt can be triggered. I could get the interrupt if the power goes below 2.3V now. 

 

0 件の賞賛
返信

1,980件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Pranavmv012 

On User Manual UM10360 Chapter 3.5 Brown-out Detection. you will find information of how is enabled and triggered. I'll look for a example code.

Let me know if you have another question.

Best Regards, Miguel.

0 件の賞賛
返信