LPC54102, SPI example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54102, SPI example

1,300 Views
etienneschaeffe
Contributor I

Hi,

In lpc5410x_xpresso54102_lpcxpresso_v3.02.000_13, it seems in periph_spi_sm_int / readme.txt :

- SPI0 MISO to SPI1 MOSI

- SPI0 MOSI to SPI1 MISO

are wrong.

It works better if : 

- SPI0 MISO to SPI1 MISO

- SPI0 MOSI to SPI1 MOSI

Regards,

0 Kudos
Reply
1 Reply

1,142 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi etienneschaeffer,

    Yes, you are correct.

    The readme.text is wrong about the description.

    SPI0 MOS1 should connect to SPI1 MOSI
   SPI0 MISO should connect to SPI1 MISO

   I will report this readme bug to the according department.

   Thank you for your inform.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply