LPC54102, SPI example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54102, SPI example

1,314 次查看
etienneschaeffe
Contributor I

Hi,

In lpc5410x_xpresso54102_lpcxpresso_v3.02.000_13, it seems in periph_spi_sm_int / readme.txt :

- SPI0 MISO to SPI1 MOSI

- SPI0 MOSI to SPI1 MISO

are wrong.

It works better if : 

- SPI0 MISO to SPI1 MISO

- SPI0 MOSI to SPI1 MOSI

Regards,

0 项奖励
回复
1 回复

1,156 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi etienneschaeffer,

    Yes, you are correct.

    The readme.text is wrong about the description.

    SPI0 MOS1 should connect to SPI1 MOSI
   SPI0 MISO should connect to SPI1 MISO

   I will report this readme bug to the according department.

   Thank you for your inform.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复