LPC54102 SPI Master clocking out extra byte

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54102 SPI Master clocking out extra byte

1,042 次查看
chrisoneill
Contributor I

Using Chip_SPIM_XferHandler(), similar to periph_spi_sm_int project, for a read function.  My example clocks out 6 bytes, then clocks in 2 bytes (for a total of 8 bytes).  Works fine @ 1 MHz.  When I increase the clock rate to 4 MHz, after clocking the correct number of bytes (8), I see a de-assert, assert, 1 more byte clocked, then a final de-assert.

Something about the interaction of the SPIMASTERIRQHANDLER(void) and the handling of tx and rx counts in Chip_SPIM_XferHandler()?

Anyone see any issues like this?

Enabling the same interrupts and options as the demo code:

Chip_SPI_EnableInts(LPC_SPIMASTERPORT,
(
SPI_INTENSET_RXDYEN |
SPI_INTENSET_RXOVEN |
SPI_INTENSET_TXUREN |
SPI_INTENSET_SSAEN |
SPI_INTENSET_SSDEN |
0
));

/* Setup master transfer options - 8 data bits per transfer, EOT, EOF */
spiMasterXfer.options =
SPIM_XFER_OPTION_SIZE(8) | /* This must be enabled as a minimum, use 8 data bits */
SPIM_XFER_OPTION_EOT | /* Enable this to assert and deassert SSEL for each individual byte/word */
SPIM_XFER_OPTION_EOF | /* Insert a delay between bytes/words as defined by frame delay time */
0;

0 项奖励
回复
0 回复数