LPC54102 Max Freq of External clock input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54102 Max Freq of External clock input

288 Views
kennethkong852
Contributor II

Hello,

I am referencing to both the User Manual and the Datasheet of LPC5410x and noticed the following:

From (User Manual) UM10850:
For clock generation, it states that External clock input can be up to 24 MHz.

From Product datasheet:
It states that External clock input for clock frequencies of up to 25 MHz.

Can you please advise which statement is correct?

Regards,

Kenneth

Labels (1)
0 Kudos
Reply
3 Replies

248 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kennethkong852 

Datasheet is correct.

External clock input for clock frequencies of up to 25 MHz.

I will escalate the UM issue to DOC team.

Thanks for your sharing.

 

BR

Alice

0 Kudos
Reply

229 Views
kennethkong852
Contributor II

Hi Alice,

Thank you for the reply and information there!  

When I use the Clocks Config Tool (accessed from SDK Builder), I noticed that for the Configurator would not allow me to type in 25 MHz for CLKIN input.  It's limited to 24 MHz.

Please see attached photo for reference.

CLKIN valuesCLKIN values

BR,

Kenneth

Tags (2)
0 Kudos
Reply

225 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kennethkong852 

Thanks for your report.
This is a bug in the Clocks Config Tool. The issue arises because the new version of DS has changed the frequency from 24M to 25M. In old version DS, still 24MHZ.
I will report this bug to the Config Tool development team promptly.
For now, if you need to use 25MHZ, please configure it via code.
I apologize for the inconvenience this has caused you.
 
BR
Alice

 

 

 

0 Kudos
Reply