LPC540XX Custom Board MCU-LINK PRO JTAG Connection Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC540XX Custom Board MCU-LINK PRO JTAG Connection Problem

6,350件の閲覧回数
mtsang
Contributor III

Hi All,

     Currently I have a MCU-LINK PRO, and I am using it as a J-Link probe. I am trying to connect my custom board (LPC54S018JET180E) to the MCU-Link Pro with J-Link Commander to test the hardware setup of my custom board. My ultimate goal is to be able upload a "Hello World" firmware to my custom board by the use of MCU-Link Pro.

     My current set up is [TMS, TDI, TDO, RESETN](PIO0_4,5,6, PIO1_24) to MCU-LINK PRO (J7_2,6,8,10) with a 10K pull up resistors. And [TCK](PIO0_3) to MCU-LINK PRO (J7_2) with a 10k pull down resistor.

     I tried to use J-Link Commander to verify the hardware setup, but I got an error message as below:

mtsang_0-1748623036943.pngmtsang_0-1748623036943.png

     Does the device selection affects the connection? Currently I selected "LPC54S018".

mtsang_1-1748623190344.pngmtsang_1-1748623190344.png

 

     Please share insight and advice on this matter.

 

Thanks,

5/30/2025

 

 

 

 

タグ(1)
0 件の賞賛
返信
14 返答(返信)

6,273件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang 

LPC540xx supports JTAG boundary scan but does not support JTAG debugging. Please use SWD debugging instead.

Thank you.

 

BR

Alice

 

0 件の賞賛
返信

6,255件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     Instead of JTAG debugging, can I use the JTAG port(PIO0_2,3,4,5,6, PIO1_24) to upload a firmware to my custom board by using a MCU-Link Pro?

     My intention is to upload a simple firmware like "Hello World" to my custom board's External SPI Flash. Also the custom board boot up by reading the external SPI Flash.

 

Thanks,

6/4/2025

0 件の賞賛
返信

6,238件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang 

Please use SWD interface. Only two pins are needed. 

Alice_Yang_0-1749092476715.pngAlice_Yang_0-1749092476715.png

 

For hardware design, you may refer to the schematic of LPC54s018-evk or the thread below:

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565  

 

BR

Alice

0 件の賞賛
返信

6,163件の閲覧回数
mtsang
Contributor III

Hi Alice,

     I am able to get the below message after I use the SWD connection. Does that mean I am able to connect to the LPC54S018JET180E? I also connected the "ResetN" from my custom board to the MCU-Link Pro's J7_10

mtsang_0-1749244907733.pngmtsang_0-1749244907733.png 

 

My next question will be how to setup the "Hello_World_qspi_xip" demo. I imported and built the example project but I get the below message instead. Is there any setting that I missed?

 

mtsang_1-1749245490306.pngmtsang_1-1749245490306.png

Executing flash operation 'Program' (Program executable into flash Debug\lpcxpresso54s018_hello_world_qspi_xip_Hello World.axf) - Fri Jun 06 14:32:17 PDT 2025

Checking MCU info...

Scanning for targets...

Executing flash action...

SEGGER J-Link Commander V8.12a (Compiled Jan 9 2025 14:39:11)

DLL version V8.12a, compiled Jan 9 2025 14:38:21

J-Link Command File read successfully.

Processing script file...

J-Link>ExitOnError 1

J-Link Commander will now exit on Error

J-Link>r

J-Link connection not established yet but required for command.

Connecting to J-Link via USB...O.K.

Firmware: J-Link MCU-Link V1 compiled Oct 9 2024 11:01:41

Hardware version: V1.00

J-Link uptime (since boot): 0d 00h 26m 20s

S/N: 1065866588

USB speed mode: High speed (480 MBit/s)

VTref=3.300V

Target connection not established yet but required for command.

Device "LPC54S018" selected.

Connecting to target via SWD

Found SW-DP with ID 0x2BA01477

DPIDR: 0x2BA01477

CoreSight SoC-400 or earlier

Scanning AP map to find all available APs

AP[1]: Stopped AP scan as end of AP map has been reached

AP[0]: AHB-AP (IDR: 0x24770011, ADDR: 0x00000000)

Iterating through AP map to find AHB-AP to use

AP[0]: Core found

AP[0]: AHB-AP ROM base: 0xE00FF000

CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)

Found Cortex-M4 r0p1, Little endian.

FPUnit: 6 code (BP) slots and 2 literal slots

CoreSight components:

ROMTbl[0] @ E00FF000

[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7

[0][1]: E0001000 CID B105E00D PID 003BB002 DWT

[0][2]: E0002000 CID B105E00D PID 002BB003 FPB

[0][3]: E0000000 CID B105E00D PID 003BB001 ITM

[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU

[0][5]: E0041000 CID B105900D PID 000BB925 ETM

Memory zones:

"Default" Description: Default access mode

Cortex-M4 identified.

Reset delay: 0 ms

ResetTarget() start

Core did not halt after reset step 2

ResetTarget() end - Took 213ms

Device specific reset executed.

AfterResetTarget() start

AfterResetTarget() end - Took 1us

J-Link>loadfile "C:\Users\tsangm\Documents\MCUXpressoIDE_24.12.148\workspace\lpcxpresso54s018_hello_world_qspi_xip_Hello World\Debug\lpcxpresso54s018_hello_world_qspi_xip_Hello World.hex" 0x10000000

'loadfile': Performing implicit reset & halt of MCU.

ResetTarget() start

Core did not halt after reset step 2

ResetTarget() end - Took 213ms

Device specific reset executed.

AfterResetTarget() start

AfterResetTarget() end - Took 2us

Downloading file [C:\Users\tsangm\Documents\MCUXpressoIDE_24.12.148\workspace\lpcxpresso54s018_hello_world_qspi_xip_Hello World\Debug\lpcxpresso54s018_hello_world_qspi_xip_Hello World.hex]...

****** Error: Failed to prepare RAMCode using RAM

Error while determining flash info (Bank @ 0x10000000)

Unspecified error -1

Script processing completed.

Unable to perform operation!

Command failed with exit code 1

 

Thanks,

6/6/2025

 

タグ(1)
0 件の賞賛
返信

6,122件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang 

Please confirm that you have selected the correct flash driver as follows:
 

Alice_Yang_0-1749438498288.pngAlice_Yang_0-1749438498288.png

 

If still has issue, please create a new MCUXpresso IDE workspace, and import new example.

Then take  a video show all your debug steps. I help you check. 

 

BR

Alice

 

0 件の賞賛
返信

6,090件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     Thank you for your response!

 

     I followed the below table during the programming. I used pull-up resistors for PIO0_4,5, and a switch to pull down PIO0_6 during the programming.

     I am using 'IS25LP128F-JBLA3' and connected it to PIO0_[23-28] on my custom board.

 

mtsang_3-1749496701997.pngmtsang_3-1749496701997.png

 

     I created an new workplace, but I am still getting the same error.

Here is my correct flash driver setting:

mtsang_0-1749495732531.pngmtsang_0-1749495732531.png

mtsang_4-1749496904437.pngmtsang_4-1749496904437.png

 

Here is the error message:

Executing flash operation 'Program' (Program file into flash: Debug\lpcxpresso54s018_hello_world_qspi_xip_Hello_World.axf) - Mon Jun 09 12:04:44 PDT 2025

Checking MCU info...

Scanning for targets...

Executing flash action...

LinkServer RedlinkMulti Driver v24.12 (Dec 18 2024 18:34:07 - crt_emu_cm_redlink.exe build 869)

( 0) Reading remote configuration

Wc(03). No cache support.

Found chip XML file in C:/Users/tsangm/Documents/MCUXpressoIDE_24.12.148/workspace/lpcxpresso54s018_hello_world_qspi_xip_Hello_World/Debug\LPC54S018.xml

( 5) Remote configuration complete

Reconnected to existing LinkServer process.

Probe Firmware: MCU-LINK Pro (r0CF) CMSIS-DAP V3.153 (NXP Semiconductors)

Serial Number: F4ON0DG121ZHK

VID:PID: 1FC9:0143

USB Path: 0001:0027:00

Using memory from core 0 after searching for a good core

On debug connection - use system reset, stalling when 0x40000040 is accessed

Retask read watchpoint 1 at 0x40000040 to use for boot ROM stall

Waiting for target to stop...

Warning - processor did not halt - gave up waiting

( 30) Emulator Connected

( 40) Debug Halt

( 50) CPU ID

debug interface type = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0

processor type = Cortex-M4 (CPU ID 00000C24) on DAP AP 0

number of h/w breakpoints = 6

number of flash patches = 2

number of h/w watchpoints = 4

Probe(0): Connected&Reset. DpID: 2BA01477. CpuID: 00000C24. Info: <None>

Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.

Content of CoreSight Debug ROM(s):

RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)

ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)

ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)

ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)

ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)

ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU

ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core

NXP: LPC54S018

DAP stride is 4096 bytes (1024 words)

Inspected v.2 External Flash Device on SPI LPC540xx_SPIFI_SFDP.cfx

Image 'LPC540xx_JEDEC_SFDP Dec 18 2024 17:26:01'

Opening flash driver LPC540xx_SPIFI_SFDP.cfx

Using SOFT reset to run the flash driver

rst - Boot ROM stall address was not accessed (but we entered debug on Halt anyway)

Driver V.2 dynamic startup failed - driver Init provided no flash parameters

Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.

Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 15 (0xF)

chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.

failed to initialize flash driver LPC540xx_SPIFI_SFDP.cfx

( 65) Chip Setup Complete

(100) Target Operation Failed

Unable to perform operation!

Command failed with exit code 1

 

Thanks,

6/9/2025

タグ(2)
0 件の賞賛
返信

6,075件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     I used the following setting in the "GUI Flash Tool", and I got the below error message. I didn't happen to lock the MCU, do I?

 

mtsang_0-1749514106615.pngmtsang_0-1749514106615.png

Executing flash operation 'Program' (Program file into flash: lpcxpresso54s018_hello_world_qspi_xip_HelloWorld000.axf) - Mon Jun 09 16:36:32 PDT 2025
Checking MCU info...
Scanning for targets...
Executing flash action...
LinkServer RedlinkMulti Driver v24.12 (Dec 18 2024 18:34:07 - crt_emu_cm_redlink.exe build 869)
( 0) Reading remote configuration
Wc(03). No cache support.
Found chip XML file in C:/Users/tsangm/Documents/MCUXpressoIDE_24.12.148/workspace/lpcxpresso54s018_hello_world_qspi_xip_HelloWorld000/Debug\LPC54S018.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
Probe Firmware: MCU-LINK Pro (r0CF) CMSIS-DAP V3.153 (NXP Semiconductors)
Serial Number: F4ON0DG121ZHK
VID:PID: 1FC9:0143
USB Path: 0001:002b:00
Using memory from core 0 after searching for a good core
On debug connection - use system reset, stalling when 0x40000040 is accessed
Retask read watchpoint 1 at 0x40000040 to use for boot ROM stall
Waiting for target to stop...
Warning - processor did not halt - gave up waiting
( 30) Emulator Connected
( 40) Debug Halt
( 50) CPU ID
debug interface type = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0
processor type = Cortex-M4 (CPU ID 00000C24) on DAP AP 0
number of h/w breakpoints = 6
number of flash patches = 2
number of h/w watchpoints = 4
Probe(0): Connected&Reset. DpID: 2BA01477. CpuID: 00000C24. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.
Content of CoreSight Debug ROM(s):
RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU
ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core
NXP: LPC54S018
DAP stride is 4096 bytes (1024 words)
Inspected v.2 External Flash Device on SPI LPC540xx_SPIFI_SFDP.cfx
Image 'LPC540xx_JEDEC_SFDP Dec 18 2024 17:26:01'
Opening flash driver LPC540xx_SPIFI_SFDP.cfx
Sending SYSRESETREQ to run flash driver
rst - Boot ROM stall address was not accessed (but we entered debug on VectorCatch anyway)
There was a problem after we succesfully downloaded flash driver code to the target, so we are going to compare the flash driver code with the memory where it was loaded.
Note that, after driver initialization, some difference is normal in 'generic' drivers.

Driver from AXF file:
00000000: 23010020 54000045 00001032 00000000 ..#E..T2.......
00000010: 0000128c 00002290 00008000 00002290 ....."......."..
00000020: 00001000 00001040 0000121c 0000009d ....@...........
00000030: 00000000 b5f74b14 60130089 49131853 .....K.....`S..I
00000040: 468c9301 4f134b12 428a9901 6c7cd019 ...F.K.O...B..|l
00000050: 1909e003 d8034281 68d93308 d1f81c4d .....B...3.hM...
00000060: 681d0001 19454c0c d10442a9 68196054 ...h.LE..B..T`.h
00000070: 18403204 780ee7e8 40743101 43744666 [email protected]@fFtC
00000080: 2000e7f2 46c0bdfe 01000001 01000193 ... ...F........
00000090: 0000127c 0000121c 811c9dc5 b6720004 |.............r.
000000A0: f86cf000 00072300 61636020 8f5ff3bf ..l..#.. `ca.._.
000000B0: 2d006965 2300d0fa 429f6123 2640d009 ei.-...##a.B..@&
000000C0: 23006027 61636126 33ff3301 d1ed429d '`.#&aca.3.3.B..
000000D0: 2308e7fe d005421d 68e16860 f8ccf000 ...#.B..`h.h....
000000E0: e0092600 002e2310 421d401e 4b21d00d .&...#[email protected]..!K
000000F0: d1072b00 00302600 28006020 2301d0e1 .+...&0. `.(...#
00000100: e7de431e f8dcf000 2342e7ea d012421d .C........B#.B..
00000110: d40807ab 2b004b18 6860d0ec 68a268e1 .....K.+..`h.h.h
00000120: f904f000 6860e7e8 68a268e1 f8d4f000 ......`h.h.h....
00000130: d0ef2800 2380e7e0 021b002e 421d401e .(.....#[email protected]
00000140: 4b0dd00d d0042b00 0039003a f0000038 ...K.+..:.9.8...
00000150: 6860f8ed 68a268e1 ff6cf7ff 23c0e7c0 ..`h.h.h..l....#
00000160: 421d005b f000d003 0038f875 0028e7c4 [..B....u.8...(.
00000170: e7c12602 000002c1 0000032d f8dfb5f8 .&......-.......
00000180: 680100d0 0170f441 48286001 feecf000 ...hA.p..`(H....
00000190: 280eb1a8 4604d002 bdf84620 48254b24 ...(...F F..$K%H
000001A0: 3280f44f 1180f44f 2103e9c3 7280f44f O..2O......!O..r
000001B0: 4921609a f8832204 f0002024 4c1dff51 .`!I."..$ ..Q..L
000001C0: f0004620 280bff6e d8104919 4e1b694f F..n..(.I..Oi.N
000001D0: 23141825 f203fa27 020ff002 5cb23b04 %..#'........;.\
000001E0: 2b01f805 d1f51d1a 23004420 4a147183 ...+.... D.#.q.J
000001F0: 6493690b 661368cb 4f80f5b3 f44fbf28 .i.d.h.f...O(.O.
00000200: 64d34380 4b10490f e9c3610b 22002400 .C.d.I.K.a...$."
00000210: 2202e9c3 22104b0d 69dc61da 0410f014 ...".K.".a.i....
00000220: 4903d1fb f0004809 e7b5fe7b c0000004 ...I.H..{.......
00000230: 000011dc 00001190 00001156 00001160 ........V...`...
00000240: 0000121c 0000a290 000011c0 40080000 ...............@
00000250: e000ed88 22104b06 61dab510 f01469dc .....K."...a.i..
00000260: d1fb0410 48024903 fe5af000 bd104620 .....I.H..Z. F..
00000270: 40080000 000011dc 5f80f1b0 41f0e92d ...@......._-..A
00000280: d316460e f8df4f0c f1008034 25004470 .F...O..4...pD.%
00000290: d10242b5 e8bd2000 68fa81f0 23004906 .B... .....h.I.#
000002A0: 4205fb02 f0004640 2800fcc5 3501d1f3 ...B@F.....(...5
000002B0: f04fe7ee e7ee30ff 000011dc 40080000 ..O..0.........@
000002C0: e9d34b04 f04f3103 fbb15080 f7fff1f3 .K...1O..P......
000002D0: bf00bfd3 000011dc 5f80f1b0 43f8e92d ..........._-..C
000002E0: 4617460c f8dfd31b f8df803c f100903c .F.F....<...<...
000002F0: 26004570 f8d8b154 490a3008 7306fb03 pE.&T....0.I...s
00000300: 4648462a fc62f000 4604b118 e8bd4620 *FHF..b....F F..
00000310: f8d883f8 36013008 441d1ae4 f04fe7ea .....0.6...D..O.
00000320: e7f334ff 000011dc 40080000 b5704b15 [email protected].
00000330: 22104616 460d4604 69da61da d4fc06d2 .F.".F.F.a.i....
00000340: 48104911 fdecf000 6c5b4b10 462a42a3 .I.H.....K[l.B*F
00000350: 2d1cd113 221cbf28 46204631 fe5ef000 ...-(.."1F F..^.
00000360: 2d20b970 f1a5d90c f1060220 f1040120 p. -.... ... ...
00000370: e8bd0020 f0004070 4631be51 e7f84620 [email protected] F..
00000380: bf00bd70 40080000 000011dc 0000121c p......@........
00000390: 4380f04f 2630f8d3 7200f442 2630f8c3 O..C..0&B..r..0&
000003A0: 2634f8d3 0208f042 2634f8c3 b5104770 ..4&B.....4&pG..
000003B0: 40c82100 f3c0d01a b2c32203 2b203a01 .!.@....."...: +
000003C0: d10db2d2 4380f04f 64dc2401 2380f503 ....O..C.$.d...#
000003D0: 2300621a d0022918 2b00310c bd10d0e9 .b.#.)...1.+....
000003E0: f103009b f8c34380 e7f2227c e7f12301 .....C..|"...#..
000003F0: f1000080 b11a4080 5300f04f 3300f8c0 [email protected]
00000400: f04fb921 f8c04380 47703300 f8c03901 !.O..C...3pG.9..
00000410: 47701300 4380f04f f8d34803 f0133610 ..pGO..C.H...6..
00000420: bf180f10 47702000 00b71b00 4280f04f ..... pG....O..B
00000430: 3610f8d2 d41102db 3508f8d2 2508f8d2 ...6.......5...%
00000440: f3c24907 f0031244 5c88031f f24c3301 .I..D......\.3L.
00000450: 43503250 fbb0005b 4770f0f3 47702000 P2PC[.....pG. pG
00000460: 00001170 4380f04f 2610f8d3 d40c06d2 p...O..C...&....
00000470: 0500f8d3 d0094018 3500f8d3 f4134804 [email protected]..
00000480: 4b044f80 4618bf18 20004770 bf004770 .O.K...FpG. pG..
00000490: 02dc6c00 05b8d800 4380f04f 2284f8d3 .l......O..C..."
000004A0: f8d3b922 b90a2280 bfb4f7ff 2284f8d3 "...."........."
000004B0: f8d3b91a 2b013280 f04fd023 f8d34380 .....2.+#.O..C..
000004C0: b92a2284 2280f8d3 d1012a02 bfaef7ff ."*....".*......
000004D0: 2284f8d3 f8d3b92a 2b033280 f7ffd101 ..."*....2.+....
000004E0: f04fbfc1 f8d34380 2a022284 4b06d102 ..O..C...".*...K
000004F0: 47706818 0284f8d3 42581ec3 03c04158 .hpG......XBXA..
00000500: 48024770 bf004770 000011d8 00b71b00 pG.HpG..........
00000510: 4380f04f 22a0f8d3 f7ffb90a f8d3bfbd O..C..."........
00000520: 2a0122a0 4b0cd102 47706818 22a0f8d3 .".*...K.hpG..."
00000530: d1012a02 e7f74b09 22a0f8d3 d1012a03 .*...K.....".*..
00000540: bf90f7ff 22a0f8d3 d1012a04 e7eb4b04 .......".*...K..
00000550: 32a0f8d3 47702000 000011d8 000011d4 ...2. pG........
00000560: 000011d0 f04fb537 46054480 3290f8d4 ....7.O..D.F...2
00000570: 0307f003 d1012b01 ff0af7ff fd3cf000 .....+........<.
00000580: 0280f44f 2620f8c4 f8c4682b 686b3580 O..... &+h...5kh
00000590: 3588f8c4 6380f443 3588f8c4 f8c468ab ...5C..c...5.h..
000005A0: f043358c f8c40380 68eb358c 3590f8c4 .5C......5.h...5
000005B0: 3300f443 3590f8c4 078869a9 f8d4d022 C..3...5.i.."...
000005C0: 48153590 0590f8c4 2630f8c4 f8c44a13 .5.H......0&.J..
000005D0: f4232590 22003300 9a019201 d9172aab .%#..3.".....*..
000005E0: 4280f04f f8c20789 f4433590 f8c23300 O..B.....5C..3..
000005F0: f44f3590 f8c20380 d5033630 3584f8d2 .5O.....06.....5
00000600: d5fb07db 4b06692a 601a2000 bd30b003 ....*i.K. .`..0.
00000610: 32019a01 bf00e7e0 00045dd2 00065dd2 ...2.....]...]..
00000620: 000011d8 2301b281 3f40f5b0 4210ea4f .......#..@?O..B
00000630: f301fa03 4a08d305 68116053 d0fc4219 .......JS`.h.B..
00000640: 00924770 4280f102 3120f8c2 1100f8d2 pG.....B.. 1....
00000650: d0fb4219 bf004770 40040000 2301b281 .B..pG.....@...#
00000660: 3f40f5b0 4210ea4f f301fa03 4909d306 ..@?O..B.......I
00000670: 680a608b 0202ea33 4770d0fb f1020092 .`.h3.....pG....
00000680: f8c24280 f8d23140 ea331100 d0fa0101 [email protected].....
00000690: bf004770 40040000 f7ffb508 e8bdffc3 pG.....@........
000006A0: f7ff4008 f64fbfdb 800373ff 8043230f [email protected]...#C.
000006B0: 7380f44f 80c38083 72032300 f04f4770 O..s.....#.rpGO.
000006C0: f44f4380 f8c36280 23102220 69c361c3 .CO..b.. ".#.a.i
000006D0: d4fc06db 78ca790b ea4306db 880a5342 .....y.x..C.BS..
000006E0: 79ca4313 7342ea43 ea43794a 788a7382 .C.yC.BsJyC..s.x
000006F0: f4020412 43132270 05d2798a 0200f402 ....p".C.y......
00000700: 7a0a4313 f0020712 43135280 47706003 .C.z.....R.C.`pG
00000710: 07db69c3 2310d504 69c361c3 d4fc06da .i.....#.a.i....
00000720: 079b69c3 880bd4fc f3c3788a ea43030d .i.......x....C.
00000730: 79ca3382 6302ea43 03d278ca 4313b292 .3.yC..c.x.....C
00000740: 0412790a 22e0f402 794a4313 f40204d2 .y.....".CJy....
00000750: 431312c0 0552798a 0260f402 60434313 ...C.yR...`..CC`
00000760: 69c34770 d4fc079a 794a790b 04d2041b pG.i.....yJy....
00000770: 12c0f402 23e0f403 79ca4313 6302ea43 .......#.C.yC..c
00000780: 0552798a 0260f402 61834313 07db69c3 .yR...`..C.a.i..
00000790: 4770d5fc f04fb530 22104380 f8c3b089 ..pG0.O..C."....
000007A0: 48142630 f7ff4c14 4814fe02 fbfaf000 0&.H.L.....H....
000007B0: 93062300 3502f240 4384f44f e9cd2162 .#[email protected]!..
000007C0: f6413501 e9cd73ff f2401303 23032005 .5A..s....@.. .#
000007D0: 94059307 fdebf7ff f7ffa801 4620fec3 .............. F
000007E0: fbe0f000 f7ff4628 4b05fde2 b009601c ....(F.....K.`..
000007F0: bf00bd30 00102101 0aba9500 00b71b00 0....!..........
00000800: 000011bc bfc6f7ff f04f4770 f44f4380 ........pGO..CO.
00000810: f8c35200 f5032220 f2405380 65da3226 .R.. "...S@.&2.e
00000820: 665a661a 66da669a f240671a 675a3201 [email protected]
00000830: 4770679a bfe9f7ff 2301b513 22004604 .gpG.......#.F."
00000840: 1007f88d 93004669 2004f8ad 3006f88d ....iF..... ...0
00000850: ff5ef7ff b0027d20 0000bd10 461fb5f7 ..^. }.........F
00000860: 46152300 f8ad460e 46693002 93014b09 .#.F.F...0iF.K..
00000870: f7ff4604 463aff76 5180f106 f0004628 .F..v.:F...Q(F..
00000880: 2310fbc9 69e061e3 0010f010 b003d1fb ...#.a.i........
00000890: bf00bdf0 5a040001 f44fb513 93003380 .......Z..O..3..
000008A0: f8ad2300 23013004 3006f88d f88d2320 .#...0.#...0 #..
000008B0: 61c31007 46044669 ff2af7ff 069b69e3 ...aiF.F..*..i..
000008C0: 7d20d5fc 0001f000 bd10b002 f04fb573 .. }........s.O.
000008D0: 93007380 460c2300 3004f8ad 46052301 .s...#.F...0.#.F
000008E0: 3006f88d 3021f891 3007f88d f7ff4669 ...0..!0...0iF..
000008F0: f894ff0f 46281020 ffcef7ff 1020f894 .... .(F...... .
00000900: 46284606 ff98f7ff 0f02f010 4630bf14 .F(F..........0F
00000910: b0022001 0000bd70 47f3e92d f891460c . ..p...-..G.F..
00000920: 4605102b d05c2900 ff86f7ff 302af894 +..F.)\.......*0
00000930: f303fa20 460707da f8dfd439 f8df80ac ......F9.......
00000940: 462190ac f7ff4628 4606ffc1 f894bb80 ..!F(F.....F....
00000950: b38b3028 1020f894 f7ff4628 f894ff6d (0.... .(F..m...
00000960: f8cd302a 22019000 f303fa02 ea40433b *0....."....;C@.
00000970: fa1f2a03 7f23fa8a 6004f8ad 46284669 .*....#....`iF(F
00000980: 2006f88d 3007f88d fec2f7ff a014f8a5 ... ...0........
00000990: 1020f894 f7ff4628 f894ff7f 4628102b .. .(F......+.(F
000009A0: ff4af7ff 302af894 07c340d8 2600d5c9 ..J...*0.@.....&
000009B0: b0024630 87f0e8bd 3004f8ad f8942601 0F.........0.&..
000009C0: f88d3029 46696006 f88d4628 f8cd3007 )0...`iF(F...0..
000009D0: f7ff8000 f894fe9d 409e302a 752e433e ........*0.@>C.u
000009E0: 2604e7d6 bf00e7e4 01000001 01000002 ...&............
000009F0: 2b0068cb f023bfb8 b5f04300 3b03bfbe .h.+..#..C.....;
00000A00: fa042401 684cf303 3301bfa4 2c3f08db .$....Lh...3..?,
00000A10: d9266103 5030f891 2d0f092d 2401d021 .a&...0P-..-!..$
00000A20: 608440ac 46252400 0c24f101 0e01f04f .@.`.$%F..$.O...
00000A30: 7014f81c fa0eb137 b1adf707 bf3c42bd ...p7........B<.
00000A40: 463d4626 2c043401 f1b3d1f2 60c57f80 &F=F.4.,.......`
00000A50: f891d91e b1533048 f8914431 70133050 ....H0S.1D..P0.p
00000A60: f44fe00d e7dc7480 463d4626 eb01e7ea ..O..t..&F=F....
00000A70: f8910146 2b203025 2bd8d006 7813d006 F...%0 +...+...x
00000A80: 3022f880 bdf02000 e7e82321 e7e623dc .."0. ..!#...#..
00000A90: 0146eb01 3025f891 0000e7e1 461eb573 ..F...%0....s..F
00000AA0: 460c781b 030ff003 618b4615 0207f10d .x.F.....F.a....
00000AB0: 46204629 ff9cf7ff f1b36923 d9387f80 )F F....#i....8.
00000AC0: f8842305 23123024 23137763 212077a3 .#..$0.#cw.#.w !
00000AD0: f3c27832 09121303 3025f884 2a02d058 2x........%0X..*
00000AE0: 7aabd12c d5120698 f0027c2a eb03031f ,..z....*|......
00000AF0: 085b1352 3026f884 f04f2920 77a303eb R.[...&0 )O....w
00000B00: f895d105 0699304c 23ecd501 682b77a3 ....L0.....#.w+h
00000B10: d8022b04 2b3f686b f895d928 f3c33042 .+..kh?+(...B0..
00000B20: 3b011302 d8462b05 f003e8df 2a3b352a ...;.+F.....*5;*
00000B30: 2304402a 3024f884 e7c92118 d1e62a01 *@.#..$0.!...*..
00000B40: 065a7aab 7caad5e3 031ff002 1352eb03 .zZ....|......R.
00000B50: f88408db 29203026 036bf04f d1d677a3 ....&0 )O.k..w..
00000B60: 304cf895 d5d206db e7cf236c f0037873 ..L0....l#..sx..
00000B70: 3b01030f d81e2b03 f003e8df 1813020d ...;.+..........
00000B80: f8842301 f8843027 f2433028 85635301 .#..'0..(0C..Sc.
00000B90: b0022000 2301bd70 3027f884 62a34b08 . ..p..#..'0.K.b
00000BA0: 2301e7f6 3027f884 e7f84b06 f8842301 ...#..'0.K...#..
00000BB0: 4b053027 2300e7f3 3027f884 bf00e7e8 '0.K...#..'0....
00000BC0: 05060100 3f073e00 35013100 41f3e92d .....>.?.1.5-..A
00000BD0: 4604688f 4690460d f7ff461e bb10fe77 .h.F.F.F.F..w...
00000BE0: ea03427b 60a30308 7380f44f 3002f8ad {B.....`O..s...0
00000BF0: 3024f895 0004f8ad 3006f88d 7f6b4669 ..$0.......0iFk.
00000C00: 3007f88d f8ad4620 f7ff7000 4633fd81 ...0 F...p....3F
00000C10: 42971b9a f895d80a 46201020 fe3cf7ff ...B.... . F..<.
00000C20: bf182800 b0022007 81f0e8bd 2b04f853 .(... ......S..+
00000C30: e7ed6162 43f7e92d 460668cf 461d460c ba..-..C.h.F.F.F
00000C40: 2b01b12b 2004d029 e8bdb003 427f83f0 +..+).. .......B
00000C50: 8022f891 9024f891 46214017 f7ff4630 .."...$..@!F0F..
00000C60: 2800fe35 f04fd1f0 f8ad7380 46690004 5..(..O..s....iF
00000C70: 60b74630 f88d9300 f88d9006 f7ff8007 0F.`............
00000C80: f894fd47 46301020 fe06f7ff d0db2800 G... .0F.....(..
00000C90: bf142d00 20082009 f891e7d6 46998023 .-... . ....#..F
00000CA0: 5780f04f b573e7d9 f8ad461d 23003000 O..W..s..F...0.#
00000CB0: f8ad4614 f8ad3002 f88d3004 23011007 .F...0...0.....#
00000CC0: 46064669 3006f88d f7ff4425 4622fd21 iF.F...0%D..!."F
00000CD0: d10742aa 61f32310 f01069f0 d1fb0010 .B...#.a.i......
00000CE0: bd70b002 f8027d33 e7f13b01 460db57f ..p.3}...;.....F
00000CF0: 200a4606 fcd0f7ff 2009f240 fb57f7ff .F. ....@.. ..W.
00000D00: fc06f7ff 290069a9 fbb0d053 2200f1f1 .....i.)S......"
00000D10: f7ff2024 f105fb6d 4630012c fccff7ff $ ..m...,.0F....
00000D20: aa012303 4825219f ffbdf7ff aa012303 .#...!%H.....#..
00000D30: 4822219f ffb7f7ff aa012303 481f219f .!"H.....#...!.H
00000D40: ffb1f7ff 0004f89d 3005f89d 1006f89d ...........0....
00000D50: 0203ea00 2aff400a 021bd02d 4300eb03 .....@.*-......C
00000D60: 616b440b 46304629 fdb0f7ff b9e84604 .Dka)F0F.....F..
00000D70: 93024b13 f8ad2301 f88d000c a902300e .K...#.......0..
00000D80: f88d7f2b 4630300f fcc2f7ff f8957534 +....00F....4u..
00000D90: 46301020 fd80f7ff b9384604 3027f895 .0F.....F8...'0
00000DA0: 4629b123 f7ff4630 4604fdb7 b0044620 #.)F0F.....F F..
00000DB0: 2404bd70 240fe7fa bf00e7f8 40080000 p..$...$.......@
00000DC0: 01000001 4ff0e92d b0af460c 46062100 ....-..O.F...!.F
00000DD0: 46204690 f0002238 f104f91f f7ff002c .F F8"......,...
00000DE0: 2305fc62 3020f884 f88423d8 23023022 b..#.. 0.#.."0.#
00000DF0: 23037763 230477a3 f8df77e3 4944a120 cw.#.w.#.w.. .DI
00000E00: f8842306 23c73021 3023f884 3004f8da .#..!0.#..#0...0
00000E10: f04f61a3 61237380 f04f4b3e e9c40b01 .aO..s#a>KO.....
00000E20: f8841300 4621b01c f7ff4630 4601ff5f ......!F0F.._..F
00000E30: d1692800 aa032308 f7ff4630 4601fd0f .(i..#..0F.....F
00000E40: d1612800 9a034b34 d15c429a 7012f89d .(a.4K...B\....p
00000E50: 3010f89d 445f9319 bf282f0a 2108270a ...0.._D./(..'.!
00000E60: aa0500fb f7ff4630 4601fcf9 d14b2800 ....0F.....F.(K.
00000E70: 22549001 f000a819 9901f8cf 4689ad05 ..T"...........F
00000E80: 782a79eb 2203eb02 4f7ff5b2 f64fd003 .y*x..."...O..O.
00000E90: 429a7384 79a9d118 ea43796b 79292301 .s.B...ykyC..#)y
00000EA0: 2103ea41 f5b278eb ea4f4f7f d1210383 A..!.x...OO...!.
00000EB0: bf282b40 aa1b2340 93014630 fccef7ff @+(.@#..0F......
00000EC0: bb084601 931a9b01 0901f109 f105454f .F..........OE..
00000ED0: d1d50508 46434621 4630aa19 fddef7ff ....!FCF..0F....
00000EE0: b9884601 3000f898 030ff003 3023f85a .F.....0....Z.#0
00000EF0: e00961a3 4630aa2c fcb0f7ff b9184601 .a..,.0F.....F..
00000F00: b0acf88d 210ee7e0 b02f4608 8ff0e8bd .......!.F/.....
00000F10: 7274736b 56010000 50444653 000011a4 kstr...VSFDP....
00000F20: 3027f891 4606b573 b9bb460d 3026f895 ..'0s..F.F....&0
00000F30: 3004f88d 3025f895 3005f88d 3024f895 ...0..%0...0..$0
00000F40: 3006f88d 7fab2400 46309400 f88d4669 ...0.$....0FiF..
00000F50: f7ff3007 4620fc06 bd70b002 fcdcf7ff .0.... F..p.....
00000F60: d0e32800 0000e7f8 4e0bb570 46044d0b .(......p..N.M.F
00000F70: fc60f7ff fc46f7ff fc46f7ff 46314a08 ..`...F...F..J1F
00000F80: 60144628 ff1ef7ff 46044631 f7ff4628 (F.`....1F.F(F..
00000F90: 4620ffc7 bf00bd70 000011dc 40080000 .. Fp..........@
00000FA0: 00001214 42984b11 d8084b11 210c220b .....K.B.K...".!
00000FB0: 6059601a 60da609a 615a611a 4a0d4770 .`Y`.`.`.aZapG.J
00000FC0: f04f4290 d807000c 210b220d 6058601a .BO......".!.`X`
00000FD0: 60da6099 e7f06119 210f220b 60586019 .`.`.a...".!.`X`
00000FE0: 60d9609a 220d611a bf00e7e7 05f5e100 .`.`.a."........
00000FF0: 40020000 0aba9500 4380f04f 6280f04f [email protected]
00001000: 2630f8c3 6d534a02 d5fc069b bf004770 ..0&.JSm....pG..
00001010: 40020000 b86cf000 b884f000 0301ea40 [email protected].....@...
00001020: b570079b 4604d10d 2a03460b 46204619 ..p....F.F.*.F F
00001030: 6806d907 42ae680d 0404f104 0304f103 ...h.h.B........
00001040: 4402d004 d1034290 e0082000 e7ec3a04 ...D.B... ...:..
00001050: 3b01f810 4b01f811 d0f342a3 bd701b18 ...;...K.B....p.
00001060: 0301ea40 b510079b 3904d113 f8514602 @..........9.FQ.
00001070: f1a33f04 ea243401 f0140403 d0053f80 .?...4$......?..
00001080: f802b2d9 b1591b01 e7f9121b 3b04f842 ......Y.....B..;
00001090: 1e42e7ed 3b01f811 3f01f802 d1f92b00 ..B....;...?.+..
000010A0: b510bd10 079a4603 d115461c f8544623 .....F...F..#FT.
000010B0: f1a22b04 ea213101 f0110102 d0f53f80 .+...1!......?..
000010C0: b199b2d1 4f7ff412 f412d00e bf140f7f .......O........
000010D0: 33034623 e0033001 f812461a b9091b01 #F.3.0...F......
000010E0: bd101a18 e7de4613 e7f33302 e7f13301 .....F...3...3..
000010F0: 0301ea40 460307db 4603d40c bf223a04 @......F...F.:".
00001100: cb04f851 cb04f843 0204f1b2 3204d2f7 Q...C..........2
00001110: 4770bf08 bf243a01 cb01f811 cb01f803 ..pG.:$.........
00001120: 4770d8f8 f0134603 d10e0f03 01fff001 ..pG.F..........
00001130: 2101ea41 4101ea41 bf243a04 1b04f843 A..!A..A.:$.C...
00001140: 0204f1b2 f102d2f9 3a010204 f803bf24 ...........:$...
00001150: e7fa1b01 454a4770 5f434544 005f4449 ....pGJEDEC_ID_.
00001160: 33323130 37363534 42413938 46454443 0123456789ABCDEF
00001170: 0f0c0800 1a181412 22201e1c 29282624 .......... "$&()
00001180: 2e2d2c2a 34323130 39383635 3d3c3b3a *,-.01245689:;<=
00001190: 4544454a 46535f43 005f5044 00000000 JEDEC_SFDP_.....
000011A0: 00000000 00000000 016e3600 02dc6c00 .........6n..l..
000011B0: 03938700 04c4b400 05b8d800 00b71b00 ................
000011C0: 00000000 00000000 00000000 00000000 ................
000011D0: 00000000 00000000 00000000 00000000 ................
000011E0: 00000000 00000000 00000000 00000000 ................
000011F0: 00000000 00000000 00000000 00000000 ................
00001200: 00000000 00000000 00000000 00000000 ................
00001210: 00000000 00000000 00000000 ............
Driver code in memory:
00000000: 20003fe0 03000145 03000b7d 03000b87 .?. E...}.......
00000010: 03000b8b 03000b8f 03000b93 ffffffff ................
00000020: ffffffff ffffffff ffffffff 03000b7f ................
00000030: 03000b81 ffffffff 03000b83 03000b85 ................
00000040: 03000135 03004829 03000135 03000135 5...)H..5...5...
00000050: 03000135 03000135 03000135 03000135 5...5...5...5...
00000060: 03000135 03000135 03000c99 03000135 5...5.......5...
00000070: 03000135 03000135 03000135 03000135 5...5...5...5...
00000080: 03000135 03000135 03000135 03000135 5...5...5...5...
00000090: 03000135 03000135 03000135 03000135 5...5...5...5...
000000A0: 03000135 03000135 03000135 03000135 5...5...5...5...
000000B0: 030095e5 03000135 03000135 03000135 ....5...5...5...
000000C0: 03000135 03000135 03000135 03000135 5...5...5...5...
000000D0: 03000135 03000135 03000135 03000135 5...5...5...5...
000000E0: 03000135 03000135 03000135 03000135 5...5...5...5...
000000F0: 03000135 03000135 03000135 030095fd 5...5...5.......
00000100: 03000135 03000135 03000135 03000135 5...5...5...5...
00000110: 03000135 03000135 03002105 03000135 5...5....!..5...
00000120: 03000135 03000135 03000135 03000135 5...5...5...5...
00000130: 03000135 47104a07 bf30b671 e7fbe7fc 5....J.Gq.0.....
00000140: e7f9e7fa 47104a02 e7f5e7f6 e7f3e7f4 .....J.G........
00000150: 030001d7 03001707 bfeef7ff bfecf7ff ................
00000160: bfeaf7ff bfe8f7ff 47704685 bfe4f7ff .........FpG....
00000170: bfe2f7ff bfe0f7ff bfdef7ff 0300f04f ............O...
00000180: 0400f04f 0500f04f 0600f04f 3a10c178 O...O...O...x..:
00000190: b401d1fc fd41f00b 68024817 5280f422 ......A..H.h"..R
000001A0: f04f6002 6c204480 6802bc01 68414695 .`O..D l...h.FAh
000001B0: f7ff4708 f7ffbfc1 f7ffbfbf f7ffbfbd .G..............
000001C0: 4668bfbb f7ff4770 f7ffbfb7 f7ffbfb5 ..hFpG..........
000001D0: f7ffbfb3 4a06bfb1 46953a1f 47104a05 .......J.:.F.J.G
000001E0: bfaaf7ff bfa8f7ff bfa6f7ff bfa4f7ff ................
000001F0: 2000ffff 03000883 40000208 ffffffff ... .......@....
00000200: 64d34380 4b10490f e9c3610b 22002400 .C.d.I.K.a...$."
00000210: 2202e9c3 22104b0d 69dc61da 0410f014 ...".K.".a.i....
00000220: 4903d1fb f0004809 e7b5fe7b c0000004 ...I.H..{.......
00000230: 000011dc 00001190 00001156 00001160 ........V...`...
00000240: 0000121c 0000a290 000011c0 40080000 ...............@
00000250: e000ed88 22104b06 61dab510 f01469dc .....K."...a.i..
00000260: d1fb0410 48024903 fe5af000 bd104620 .....I.H..Z. F..
00000270: 40080000 000011dc 5f80f1b0 41f0e92d ...@......._-..A
00000280: d316460e f8df4f0c f1008034 25004470 .F...O..4...pD.%
00000290: d10242b5 e8bd2000 68fa81f0 23004906 .B... .....h.I.#
000002A0: 4205fb02 f0004640 2800fcc5 3501d1f3 ...B@F.....(...5
000002B0: f04fe7ee e7ee30ff 000011dc 40080000 ..O..0.........@
000002C0: e9d34b04 f04f3103 fbb15080 f7fff1f3 .K...1O..P......
000002D0: bf00bfd3 000011dc 5f80f1b0 43f8e92d ..........._-..C
000002E0: 4617460c f8dfd31b f8df803c f100903c .F.F....<...<...
000002F0: 26004570 f8d8b154 490a3008 7306fb03 pE.&T....0.I...s
00000300: 4648462a fc62f000 4604b118 e8bd4620 *FHF..b....F F..
00000310: f8d883f8 36013008 441d1ae4 f04fe7ea .....0.6...D..O.
00000320: e7f334ff 000011dc 40080000 b5704b15 [email protected].
00000330: 22104616 460d4604 69da61da d4fc06d2 .F.".F.F.a.i....
00000340: 48104911 fdecf000 6c5b4b10 462a42a3 .I.H.....K[l.B*F
00000350: 2d1cd113 221cbf28 46204631 fe5ef000 ...-(.."1F F..^.
00000360: 2d20b970 f1a5d90c f1060220 f1040120 p. -.... ... ...
00000370: e8bd0020 f0004070 4631be51 e7f84620 [email protected] F..
00000380: bf00bd70 40080000 000011dc 0000121c p......@........
00000390: 4380f04f 2630f8d3 7200f442 2630f8c3 O..C..0&B..r..0&
000003A0: 2634f8d3 0208f042 2634f8c3 b5104770 ..4&B.....4&pG..
000003B0: 40c82100 f3c0d01a b2c32203 2b203a01 .!.@....."...: +
000003C0: d10db2d2 4380f04f 64dc2401 2380f503 ....O..C.$.d...#
000003D0: 2300621a d0022918 2b00310c bd10d0e9 .b.#.)...1.+....
000003E0: f103009b f8c34380 e7f2227c e7f12301 .....C..|"...#..
000003F0: f1000080 b11a4080 5300f04f 3300f8c0 [email protected]
00000400: f04fb921 f8c04380 47703300 f8c03901 !.O..C...3pG.9..
00000410: 47701300 4380f04f f8d34803 f0133610 ..pGO..C.H...6..
00000420: bf180f10 47702000 00b71b00 4280f04f ..... pG....O..B
00000430: 3610f8d2 d41102db 3508f8d2 2508f8d2 ...6.......5...%
00000440: f3c24907 f0031244 5c88031f f24c3301 .I..D......\.3L.
00000450: 43503250 fbb0005b 4770f0f3 47702000 P2PC[.....pG. pG
00000460: 00001170 4380f04f 2610f8d3 d40c06d2 p...O..C...&....
00000470: 0500f8d3 d0094018 3500f8d3 f4134804 [email protected]..
00000480: 4b044f80 4618bf18 20004770 bf004770 .O.K...FpG. pG..
00000490: 02dc6c00 05b8d800 4380f04f 2284f8d3 .l......O..C..."
000004A0: f8d3b922 b90a2280 bfb4f7ff 2284f8d3 "...."........."
000004B0: f8d3b91a 2b013280 f04fd023 f8d34380 .....2.+#.O..C..
000004C0: b92a2284 2280f8d3 d1012a02 bfaef7ff ."*....".*......
000004D0: 2284f8d3 f8d3b92a 2b033280 f7ffd101 ..."*....2.+....
000004E0: f04fbfc1 f8d34380 2a022284 4b06d102 ..O..C...".*...K
000004F0: 47706818 0284f8d3 42581ec3 03c04158 .hpG......XBXA..
00000500: 48024770 bf004770 000011d8 00b71b00 pG.HpG..........
00000510: 4380f04f 22a0f8d3 f7ffb90a f8d3bfbd O..C..."........
00000520: 2a0122a0 4b0cd102 47706818 22a0f8d3 .".*...K.hpG..."
00000530: d1012a02 e7f74b09 22a0f8d3 d1012a03 .*...K.....".*..
00000540: bf90f7ff 22a0f8d3 d1012a04 e7eb4b04 .......".*...K..
00000550: 32a0f8d3 47702000 000011d8 000011d4 ...2. pG........
00000560: 000011d0 f04fb537 46054480 3290f8d4 ....7.O..D.F...2
00000570: 0307f003 d1012b01 ff0af7ff fd3cf000 .....+........<.
00000580: 0280f44f 2620f8c4 f8c4682b 686b3580 O..... &+h...5kh
00000590: 3588f8c4 6380f443 3588f8c4 f8c468ab ...5C..c...5.h..
000005A0: f043358c f8c40380 68eb358c 3590f8c4 .5C......5.h...5
000005B0: 3300f443 3590f8c4 078869a9 f8d4d022 C..3...5.i.."...
000005C0: 48153590 0590f8c4 2630f8c4 f8c44a13 .5.H......0&.J..
000005D0: f4232590 22003300 9a019201 d9172aab .%#..3.".....*..
000005E0: 4280f04f f8c20789 f4433590 f8c23300 O..B.....5C..3..
000005F0: f44f3590 f8c20380 d5033630 3584f8d2 .5O.....06.....5
00000600: d5fb07db 4b06692a 601a2000 bd30b003 ....*i.K. .`..0.
00000610: 32019a01 bf00e7e0 00045dd2 00065dd2 ...2.....]...]..
00000620: 000011d8 2301b281 3f40f5b0 4210ea4f .......#..@?O..B
00000630: f301fa03 4a08d305 68116053 d0fc4219 .......JS`.h.B..
00000640: 00924770 4280f102 3120f8c2 1100f8d2 pG.....B.. 1....
00000650: d0fb4219 bf004770 40040000 2301b281 .B..pG.....@...#
00000660: 3f40f5b0 4210ea4f f301fa03 4909d306 ..@?O..B.......I
00000670: 680a608b 0202ea33 4770d0fb f1020092 .`.h3.....pG....
00000680: f8c24280 f8d23140 ea331100 d0fa0101 [email protected].....
00000690: bf004770 40040000 f7ffb508 e8bdffc3 pG.....@........
000006A0: f7ff4008 f64fbfdb 800373ff 8043230f [email protected]...#C.
000006B0: 7380f44f 80c38083 72032300 f04f4770 O..s.....#.rpGO.
000006C0: f44f4380 f8c36280 23102220 69c361c3 .CO..b.. ".#.a.i
000006D0: d4fc06db 78ca790b ea4306db 880a5342 .....y.x..C.BS..
000006E0: 79ca4313 7342ea43 ea43794a 788a7382 .C.yC.BsJyC..s.x
000006F0: f4020412 43132270 05d2798a 0200f402 ....p".C.y......
00000700: 7a0a4313 f0020712 43135280 47706003 .C.z.....R.C.`pG
00000710: 07db69c3 2310d504 69c361c3 d4fc06da .i.....#.a.i....
00000720: 079b69c3 880bd4fc f3c3788a ea43030d .i.......x....C.
00000730: 79ca3382 6302ea43 03d278ca 4313b292 .3.yC..c.x.....C
00000740: 0412790a 22e0f402 794a4313 f40204d2 .y.....".CJy....
00000750: 431312c0 0552798a 0260f402 60434313 ...C.yR...`..CC`
00000760: 69c34770 d4fc079a 794a790b 04d2041b pG.i.....yJy....
00000770: 12c0f402 23e0f403 79ca4313 6302ea43 .......#.C.yC..c
00000780: 0552798a 0260f402 61834313 07db69c3 .yR...`..C.a.i..
00000790: 4770d5fc f04fb530 22104380 f8c3b089 ..pG0.O..C."....
000007A0: 48142630 f7ff4c14 4814fe02 fbfaf000 0&.H.L.....H....
000007B0: 93062300 3502f240 4384f44f e9cd2162 .#[email protected]!..
000007C0: f6413501 e9cd73ff f2401303 23032005 .5A..s....@.. .#
000007D0: 94059307 fdebf7ff f7ffa801 4620fec3 .............. F
000007E0: fbe0f000 f7ff4628 4b05fde2 b009601c ....(F.....K.`..
000007F0: bf00bd30 00102101 0aba9500 00b71b00 0....!..........
00000800: 000011bc bfc6f7ff f04f4770 f44f4380 ........pGO..CO.
00000810: f8c35200 f5032220 f2405380 65da3226 .R.. "...S@.&2.e
00000820: 665a661a 66da669a f240671a 675a3201 [email protected]
00000830: 4770679a bfe9f7ff 2301b513 22004604 .gpG.......#.F."
00000840: 1007f88d 93004669 2004f8ad 3006f88d ....iF..... ...0
00000850: ff5ef7ff b0027d20 0000bd10 461fb5f7 ..^. }.........F
00000860: 46152300 f8ad460e 46693002 93014b09 .#.F.F...0iF.K..
00000870: f7ff4604 463aff76 5180f106 f0004628 .F..v.:F...Q(F..
00000880: 2310fbc9 69e061e3 0010f010 b003d1fb ...#.a.i........
00000890: bf00bdf0 5a040001 f44fb513 93003380 .......Z..O..3..
000008A0: f8ad2300 23013004 3006f88d f88d2320 .#...0.#...0 #..
000008B0: 61c31007 46044669 ff2af7ff 069b69e3 ...aiF.F..*..i..
000008C0: 7d20d5fc 0001f000 bd10b002 f04fb573 .. }........s.O.
000008D0: 93007380 460c2300 3004f8ad 46052301 .s...#.F...0.#.F
000008E0: 3006f88d 3021f891 3007f88d f7ff4669 ...0..!0...0iF..
000008F0: f894ff0f 46281020 ffcef7ff 1020f894 .... .(F...... .
00000900: 46284606 ff98f7ff 0f02f010 4630bf14 .F(F..........0F
00000910: b0022001 0000bd70 47f3e92d f891460c . ..p...-..G.F..
00000920: 4605102b d05c2900 ff86f7ff 302af894 +..F.)\.......*0
00000930: f303fa20 460707da f8dfd439 f8df80ac ......F9.......
00000940: 462190ac f7ff4628 4606ffc1 f894bb80 ..!F(F.....F....
00000950: b38b3028 1020f894 f7ff4628 f894ff6d (0.... .(F..m...
00000960: f8cd302a 22019000 f303fa02 ea40433b *0....."....;C@.
00000970: fa1f2a03 7f23fa8a 6004f8ad 46284669 .*....#....`iF(F
00000980: 2006f88d 3007f88d fec2f7ff a014f8a5 ... ...0........
00000990: 1020f894 f7ff4628 f894ff7f 4628102b .. .(F......+.(F
000009A0: ff4af7ff 302af894 07c340d8 2600d5c9 ..J...*0.@.....&
000009B0: b0024630 87f0e8bd 3004f8ad f8942601 0F.........0.&..
000009C0: f88d3029 46696006 f88d4628 f8cd3007 )0...`iF(F...0..
000009D0: f7ff8000 f894fe9d 409e302a 752e433e ........*0.@>C.u
000009E0: 2604e7d6 bf00e7e4 01000001 01000002 ...&............
000009F0: 2b0068cb f023bfb8 b5f04300 3b03bfbe .h.+..#..C.....;
00000A00: fa042401 684cf303 3301bfa4 2c3f08db .$....Lh...3..?,
00000A10: d9266103 5030f891 2d0f092d 2401d021 .a&...0P-..-!..$
00000A20: 608440ac 46252400 0c24f101 0e01f04f .@.`.$%F..$.O...
00000A30: 7014f81c fa0eb137 b1adf707 bf3c42bd ...p7........B<.
00000A40: 463d4626 2c043401 f1b3d1f2 60c57f80 &F=F.4.,.......`
00000A50: f891d91e b1533048 f8914431 70133050 ....H0S.1D..P0.p
00000A60: f44fe00d e7dc7480 463d4626 eb01e7ea ..O..t..&F=F....
00000A70: f8910146 2b203025 2bd8d006 7813d006 F...%0 +...+...x
00000A80: 3022f880 bdf02000 e7e82321 e7e623dc .."0. ..!#...#..
00000A90: 0146eb01 3025f891 0000e7e1 461eb573 ..F...%0....s..F
00000AA0: 460c781b 030ff003 618b4615 0207f10d .x.F.....F.a....
00000AB0: 46204629 ff9cf7ff f1b36923 d9387f80 )F F....#i....8.
00000AC0: f8842305 23123024 23137763 212077a3 .#..$0.#cw.#.w !
00000AD0: f3c27832 09121303 3025f884 2a02d058 2x........%0X..*
00000AE0: 7aabd12c d5120698 f0027c2a eb03031f ,..z....*|......
00000AF0: 085b1352 3026f884 f04f2920 77a303eb R.[...&0 )O....w
00000B00: f895d105 0699304c 23ecd501 682b77a3 ....L0.....#.w+h
00000B10: d8022b04 2b3f686b f895d928 f3c33042 .+..kh?+(...B0..
00000B20: 3b011302 d8462b05 f003e8df 2a3b352a ...;.+F.....*5;*
00000B30: 2304402a 3024f884 e7c92118 d1e62a01 *@.#..$0.!...*..
00000B40: 065a7aab 7caad5e3 031ff002 1352eb03 .zZ....|......R.
00000B50: f88408db 29203026 036bf04f d1d677a3 ....&0 )O.k..w..
00000B60: 304cf895 d5d206db e7cf236c f0037873 ..L0....l#..sx..
00000B70: 3b01030f d81e2b03 f003e8df 1813020d ...;.+..........
00000B80: f8842301 f8843027 f2433028 85635301 .#..'0..(0C..Sc.
00000B90: b0022000 2301bd70 3027f884 62a34b08 . ..p..#..'0.K.b
00000BA0: 2301e7f6 3027f884 e7f84b06 f8842301 ...#..'0.K...#..
00000BB0: 4b053027 2300e7f3 3027f884 bf00e7e8 '0.K...#..'0....
00000BC0: 05060100 3f073e00 35013100 41f3e92d .....>.?.1.5-..A
00000BD0: 4604688f 4690460d f7ff461e bb10fe77 .h.F.F.F.F..w...
00000BE0: ea03427b 60a30308 7380f44f 3002f8ad {B.....`O..s...0
00000BF0: 3024f895 0004f8ad 3006f88d 7f6b4669 ..$0.......0iFk.
00000C00: 3007f88d f8ad4620 f7ff7000 4633fd81 ...0 F...p....3F
00000C10: 42971b9a f895d80a 46201020 fe3cf7ff ...B.... . F..<.
00000C20: bf182800 b0022007 81f0e8bd 2b04f853 .(... ......S..+
00000C30: e7ed6162 43f7e92d 460668cf 461d460c ba..-..C.h.F.F.F
00000C40: 2b01b12b 2004d029 e8bdb003 427f83f0 +..+).. .......B
00000C50: 8022f891 9024f891 46214017 f7ff4630 .."...$..@!F0F..
00000C60: 2800fe35 f04fd1f0 f8ad7380 46690004 5..(..O..s....iF
00000C70: 60b74630 f88d9300 f88d9006 f7ff8007 0F.`............
00000C80: f894fd47 46301020 fe06f7ff d0db2800 G... .0F.....(..
00000C90: bf142d00 20082009 f891e7d6 46998023 .-... . ....#..F
00000CA0: 5780f04f b573e7d9 f8ad461d 23003000 O..W..s..F...0.#
00000CB0: f8ad4614 f8ad3002 f88d3004 23011007 .F...0...0.....#
00000CC0: 46064669 3006f88d f7ff4425 4622fd21 iF.F...0%D..!."F
00000CD0: d10742aa 61f32310 f01069f0 d1fb0010 .B...#.a.i......
00000CE0: bd70b002 f8027d33 e7f13b01 460db57f ..p.3}...;.....F
00000CF0: 200a4606 fcd0f7ff 2009f240 fb57f7ff .F. ....@.. ..W.
00000D00: fc06f7ff 290069a9 fbb0d053 2200f1f1 .....i.)S......"
00000D10: f7ff2024 f105fb6d 4630012c fccff7ff $ ..m...,.0F....
00000D20: aa012303 4825219f ffbdf7ff aa012303 .#...!%H.....#..
00000D30: 4822219f ffb7f7ff aa012303 481f219f .!"H.....#...!.H
00000D40: ffb1f7ff 0004f89d 3005f89d 1006f89d ...........0....
00000D50: 0203ea00 2aff400a 021bd02d 4300eb03 .....@.*-......C
00000D60: 616b440b 46304629 fdb0f7ff b9e84604 .Dka)F0F.....F..
00000D70: 93024b13 f8ad2301 f88d000c a902300e .K...#.......0..
00000D80: f88d7f2b 4630300f fcc2f7ff f8957534 +....00F....4u..
00000D90: 46301020 fd80f7ff b9384604 3027f895 .0F.....F8...'0
00000DA0: 4629b123 f7ff4630 4604fdb7 b0044620 #.)F0F.....F F..
00000DB0: 2404bd70 240fe7fa bf00e7f8 40080000 p..$...$.......@
00000DC0: 01000001 4ff0e92d b0af460c 46062100 ....-..O.F...!.F
00000DD0: 46204690 f0002238 f104f91f f7ff002c .F F8"......,...
00000DE0: 2305fc62 3020f884 f88423d8 23023022 b..#.. 0.#.."0.#
00000DF0: 23037763 230477a3 f8df77e3 4944a120 cw.#.w.#.w.. .DI
00000E00: f8842306 23c73021 3023f884 3004f8da .#..!0.#..#0...0
00000E10: f04f61a3 61237380 f04f4b3e e9c40b01 .aO..s#a>KO.....
00000E20: f8841300 4621b01c f7ff4630 4601ff5f ......!F0F.._..F
00000E30: d1692800 aa032308 f7ff4630 4601fd0f .(i..#..0F.....F
00000E40: d1612800 9a034b34 d15c429a 7012f89d .(a.4K...B\....p
00000E50: 3010f89d 445f9319 bf282f0a 2108270a ...0.._D./(..'.!
00000E60: aa0500fb f7ff4630 4601fcf9 d14b2800 ....0F.....F.(K.
00000E70: 22549001 f000a819 9901f8cf 4689ad05 ..T"...........F
00000E80: 782a79eb 2203eb02 4f7ff5b2 f64fd003 .y*x..."...O..O.
00000E90: 429a7384 79a9d118 ea43796b 79292301 .s.B...ykyC..#)y
00000EA0: 2103ea41 f5b278eb ea4f4f7f d1210383 A..!.x...OO...!.
00000EB0: bf282b40 aa1b2340 93014630 fccef7ff @+(.@#..0F......
00000EC0: bb084601 931a9b01 0901f109 f105454f .F..........OE..
00000ED0: d1d50508 46434621 4630aa19 fddef7ff ....!FCF..0F....
00000EE0: b9884601 3000f898 030ff003 3023f85a .F.....0....Z.#0
00000EF0: e00961a3 4630aa2c fcb0f7ff b9184601 .a..,.0F.....F..
00000F00: b0acf88d 210ee7e0 b02f4608 8ff0e8bd .......!.F/.....
00000F10: 7274736b 56010000 50444653 000011a4 kstr...VSFDP....
00000F20: 3027f891 4606b573 b9bb460d 3026f895 ..'0s..F.F....&0
00000F30: 3004f88d 3025f895 3005f88d 3024f895 ...0..%0...0..$0
00000F40: 3006f88d 7fab2400 46309400 f88d4669 ...0.$....0FiF..
00000F50: f7ff3007 4620fc06 bd70b002 fcdcf7ff .0.... F..p.....
00000F60: d0e32800 0000e7f8 4e0bb570 46044d0b .(......p..N.M.F
00000F70: fc60f7ff fc46f7ff fc46f7ff 46314a08 ..`...F...F..J1F
00000F80: 60144628 ff1ef7ff 46044631 f7ff4628 (F.`....1F.F(F..
00000F90: 4620ffc7 bf00bd70 000011dc 40080000 .. Fp..........@
00000FA0: 00001214 42984b11 d8084b11 210c220b .....K.B.K...".!
00000FB0: 6059601a 60da609a 615a611a 4a0d4770 .`Y`.`.`.aZapG.J
00000FC0: f04f4290 d807000c 210b220d 6058601a .BO......".!.`X`
00000FD0: 60da6099 e7f06119 210f220b 60586019 .`.`.a...".!.`X`
00000FE0: 60d9609a 220d611a bf00e7e7 05f5e100 .`.`.a."........
00000FF0: 40020000 0aba9500 4380f04f 6280f04f [email protected]
00001000: 2630f8c3 6d534a02 d5fc069b bf004770 ..0&.JSm....pG..
00001010: 40020000 b86cf000 b884f000 0301ea40 [email protected].....@...
00001020: b570079b 4604d10d 2a03460b 46204619 ..p....F.F.*.F F
00001030: 6806d907 42ae680d 0404f104 0304f103 ...h.h.B........
00001040: 4402d004 d1034290 e0082000 e7ec3a04 ...D.B... ...:..
00001050: 3b01f810 4b01f811 d0f342a3 bd701b18 ...;...K.B....p.
00001060: 0301ea40 b510079b 3904d113 f8514602 @..........9.FQ.
00001070: f1a33f04 ea243401 f0140403 d0053f80 .?...4$......?..
00001080: f802b2d9 b1591b01 e7f9121b 3b04f842 ......Y.....B..;
00001090: 1e42e7ed 3b01f811 3f01f802 d1f92b00 ..B....;...?.+..
000010A0: b510bd10 079a4603 d115461c f8544623 .....F...F..#FT.
000010B0: f1a22b04 ea213101 f0110102 d0f53f80 .+...1!......?..
000010C0: b199b2d1 4f7ff412 f412d00e bf140f7f .......O........
000010D0: 33034623 e0033001 f812461a b9091b01 #F.3.0...F......
000010E0: bd101a18 e7de4613 e7f33302 e7f13301 .....F...3...3..
000010F0: 0301ea40 460307db 4603d40c bf223a04 @......F...F.:".
00001100: cb04f851 cb04f843 0204f1b2 3204d2f7 Q...C..........2
00001110: 4770bf08 bf243a01 cb01f811 cb01f803 ..pG.:$.........
00001120: 4770d8f8 f0134603 d10e0f03 01fff001 ..pG.F..........
00001130: 2101ea41 4101ea41 bf243a04 1b04f843 A..!A..A.:$.C...
00001140: 0204f1b2 f102d2f9 3a010204 f803bf24 ...........:$...
00001150: e7fa1b01 454a4770 5f434544 005f4449 ....pGJEDEC_ID_.
00001160: 33323130 37363534 42413938 46454443 0123456789ABCDEF
00001170: 0f0c0800 1a181412 22201e1c 29282624 .......... "$&()
00001180: 2e2d2c2a 34323130 39383635 3d3c3b3a *,-.01245689:;<=
00001190: 4544454a 46535f43 005f5044 00000000 JEDEC_SFDP_.....
000011A0: 00000000 00000000 016e3600 02dc6c00 .........6n..l..
000011B0: 03938700 04c4b400 05b8d800 00b71b00 ................
000011C0: 00000000 00000000 00000000 00000000 ................
000011D0: 00000000 00000000 00000000 00000000 ................
000011E0: 00000000 00000000 00000000 00000000 ................
000011F0: 00000000 00000000 00000000 00000000 ................
00001200: 00000000 00000000 00000000 00000000 ................
00001210: 00000000 00000000 00000000 ............
AFTER driver startup timeout (302 5ms retries)
Driver Addresses
Start: 00000000
Entry: 0000009D
End: 0000128C
Stack: 00002290
Mailbox:0000A290
Driver Register State
R0: 00000000
R1: 200273F8
R2: 030095A1
R3: 00000000
R4: 40000000
R5: 00000000
R6: 00000000
R7: 00000000
R8: 00000000
R9: 00000000
R10: 00000000
R11: 00000000
R12: 00000000
SP: 00002288
LR: 0300BBA5
PC: 0300BDF2
xPSR: 21000000
MSP: 00002288
PSP: 00002290
CFBP: 00000001 (CONTROL=0x0, FAULTMASK=0x0, BASEPRI=0x0, PRIMASK=0x1)
Flash Driver V.2 startup failed - rc Ef(34): Timed-out initializing flash.
chip initialization failed - Ef(34): Timed-out initializing flash.
failed to initialize flash driver LPC540xx_SPIFI_SFDP.cfx
( 65) Chip Setup Complete
(100) Target Operation Failed
Unable to perform operation!
Command failed with exit code 1

Thanks,

6/9/2025

0 件の賞賛
返信

6,062件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang 

I recommend testing the debug functionality first in RAM to ensure it works properly. Please import the "hello_world" demo instead of "hello_world_qspi_xip", and debug it without making any changes.

If it functions correctly,  then debug  "hello_world_qspi_xip" demo without making any changes. and, configure the hardware board as follows:

Alice_Yang_0-1749536373788.pngAlice_Yang_0-1749536373788.png

BR

Alice

 

 

 

0 件の賞賛
返信

6,038件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     I imported the "hello_world" demo and I didnt make any change at all. And here is the result I got:

mtsang_0-1749600017737.pngmtsang_0-1749600017737.pngScreenshot 2025-06-10 170249.pngScreenshot 2025-06-10 170249.png

 

     Does it count as a successfully uploading?

Thanks,

6/10/2025

0 件の賞賛
返信

6,037件の閲覧回数
mtsang
Contributor III
Can it be "LPC54S018JET180E" does no have an internal flash which caused the problem?
0 件の賞賛
返信

6,017件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang

This "Hello World" demo is being debugged in RAM.

Please provide your schematic.'

 

BR

Alice

 

0 件の賞賛
返信

5,891件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     I see that from the LPC54S018 SDK, the dev board has both external QSPI(W25Q128JVFIM) and external SDRAM(W9812G6JB-6I).

     Since my custom board only has an external external SPI NOR Flash, do I need to adjust the memory in the "Project Setting"? Is there a SDK/example that is for LPC54S018JET180E and an external flash(IS25LP128F-JBLA3) only?

 

SDK, Example I am using:

mtsang_0-1749831299485.pngmtsang_0-1749831299485.png

mtsang_1-1749832010147.pngmtsang_1-1749832010147.png

mtsang_2-1749832051655.pngmtsang_2-1749832051655.png

 

Thanks,

6/13/2025

 

0 件の賞賛
返信

5,629件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mtsang 

Please create a new project based on LPC54s018, not SDK demo. Then debug. It only uses Internal RAM.

BR

Alice

0 件の賞賛
返信

5,992件の閲覧回数
mtsang
Contributor III

Hi Alice,

 

     Attached is the schematic of my custom daughter board.

 

LPC54S018 Daughter Board.jpgLPC54S018 Daughter Board.jpg

 

Thanks,

6/11/2025

タグ(2)
0 件の賞賛
返信