LPC54018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54018

2,032件の閲覧回数
bingw
Contributor I

Hi:

      Where could I get the software tools to download bin or hex file to LPC54018 borad through LPC-Link 2 and JLINK?

      Thank you! 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,901件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

If you have a J-link (or are using the J-link image of the development board) you can get the associated utilities for that from the SEGGER site:

SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace 

Not all the utilities will work with the J-link OB / Jlink for LPC-Link2, but  the J-flash lite will, and can be used to program binary images, including programming of the off-chip flash.

The MCUXpresso IDE also includes a binary / AXF file programmer.

0 件の賞賛
返信

1,901件の閲覧回数
bingw
Contributor I

Thank you very much.It work now.

0 件の賞賛
返信

1,901件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

Pls refer to the application note with the link:

https://www.nxp.com/docs/en/nxp/application-notes/AN12352.pdf 

Hope it can help you

BR

Xiangjun rong

0 件の賞賛
返信