LPC54018 uart receive FIFO overflow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018 uart receive FIFO overflow

1,831 Views
kiryat8
Contributor III

On our custom LPC54018 board, we need to use simultaneously 6 uart channels.

Our modem runs at 115,200 BPS and I am getting FIFO receive overflow errors and losing characters in the modem initialization stage. Since the modem response in not a constant length, I need to get an interrupt for every incoming character (In the interrupt I empty the rx buffer in any case). I tried disabling all other uart channels but I am still getting the overflow errors. I tried changing the watermark from kUSART_RxFifo1 to kUSART_RxFifo8, setting the uart interrupt priority to 3, using BOARD_BootClockFROHF96M() and also BOARD_BootClockPLL180M(), without resolving the problem. I can see that the modem's CTS line is low but also tried without using it.

 I tried directly using the uart interrupt with my own ring buffer and also using the uart driver with its ring buffer.

I have already looked at the SDK uart examples.

Anyone can help or see a problem in the attached code?

Labels (2)
0 Kudos
Reply
1 Reply

1,673 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David Kaplan ,

Which IDE and version do you used ? Could you please send your whole project, that I will try to

reproduce the problem on my side and analyze it.

BR

Alice

0 Kudos
Reply