LPC54018 - Program Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54018 - Program Flash

1,903件の閲覧回数
Dhaya
Contributor III

Hi,

    We are wants to flash the chip LPC 54018 with help of ULink2, but while try to add device in flash download options it shows only Ext. SPI flash and there is no On chip Flash option. How can we move further. Kindly help me

0 件の賞賛
返信
3 返答(返信)

1,874件の閲覧回数
Dhaya
Contributor III

Hi,

  Kindly help to flash the controller LPC54018. Ulink is not detected in both SW/JTAG mode since On chip flash is not available in LPC54018. Tell us the ways and procedure to flash the code other than USB mode (ISP, Ulink chain,...)

0 件の賞賛
返信

1,866件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I suggest reviewing the boot mode if you are in DFU mode. In Table 5. Boot mode based on OTP BOOT_SRC bits (10:9, bank 3, word 0), from the User manual. Or if you are using the EVK please review the state of the switch.

Pavel_Hernandez_1-1662142177756.pngPavel_Hernandez_1-1662142177756.png

Best regards,
Pavel

 

 

 

 

0 件の賞賛
返信

1,896件の閲覧回数
frank_m
Senior Contributor III

ULink2 is a Keil product.

Check the Keil website downloads, and/or Keil's uVision IDE. The latter definitely supports both LPC54xxx and ULink2.

0 件の賞賛
返信