LPC54018 I2s Config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018 I2s Config

3,894 Views
Sukumar_M
Contributor I

Hi,

I'm newly working on I2s I should try to do demo driver flash to evk but it not work how can achieve configration. please any one help me.

0 Kudos
Reply
7 Replies

3,877 Views
Sukumar_M
Contributor I

i2s interrupt transfer demo if any other option to use polling method

0 Kudos
Reply

3,869 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sukumar_M,

I test the I2S demo on my side, it can works well. So recommend you first do not change anything with demo.

 

BR

Alice

0 Kudos
Reply

3,867 Views
Sukumar_M
Contributor I

ok how to choose frequency divider value as per music. I can choose same frequency divider value multiple music is it possible

0 Kudos
Reply

3,835 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

About I2S sample rate configuration, you can refer to:

UM11060 -> 29.8.3.2 Rate calculations  

 

0 Kudos
Reply

3,882 Views
Sukumar_M
Contributor I

already one demo are there in MCUxpresso but it not work only noise are occur no sound data should be transfer.

0 Kudos
Reply

3,880 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Which demo you used? Have you configure well refer to readme? Do you use DEMO board from NXP? 

 

BR

Alice

Tags (1)
0 Kudos
Reply

3,888 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Recommend download SDK , there is I2s demo, and there is  readme.txt under project folder about how to use demo:

https://mcuxpresso.nxp.com/en/builder?hw=LPCXpresso54018  

 

 

BR

Alice

0 Kudos
Reply