LPC54018 ADC 16-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018 ADC 16-bit

3,795 Views
Sukumar_M
Contributor I

Hi,

Why LPC54018 Microcontroller have 16-bit ADC. As per data Sheet it should be configure only 12 bit but its resolution is 16 bit the final stage of function it should be shifted.

Why?

0 Kudos
Reply
7 Replies

3,788 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the following screenshot from UM11060.pdf,the ADC resolution for LPC540xx is 12 bits instead of 16 bits.

where did you know the ADC resolution is 16 bits?

 

BR

XiangJun Rong

 

xiangjun_rong_0-1657193269421.png

 

0 Kudos
Reply

3,777 Views
frank_m
Senior Contributor III

If I remember correctly, the 12-bit result of the ADC is left-aligned within the result register.

0 Kudos
Reply

3,781 Views
Sukumar_M
Contributor I

Hi 

I'm worked in mcuxpresso Its configered as per data sheet is 12 bit but its shifted from this deriverd value originally its 16 bit.

from given below example:

Capture1.JPGCapture.JPG

Tags (1)
0 Kudos
Reply

3,774 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sukumar,

The ADC data register is 32 bits, but the 12 bits sample result occupies 4~15 bits, as a uint16_t variable format, it is a left-alignment data as Frank said.

For detailed inf,pls refer to section 43.6.6 ADC Channel Data registers 0 to 11 in UM11155.pdf.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1657262129409.png

 

0 Kudos
Reply

3,743 Views
Sukumar_M
Contributor I

OK,

If may use 16 bit ADC any issue

0 Kudos
Reply

3,734 Views
frank_m
Senior Contributor III

> If may use 16 bit ADC any issue

I don't understand what actually the question is.

But proper PCB design for a 16-bit ADC is not trivial. A bad design can have worse accuracy and performance values than a proper 12-bit design.

My company uses 10-bit and 12-bit ADC inputs in control units for safety-certified heavy machinery.

0 Kudos
Reply

3,737 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the ADC of LPC54018 has only fixed 12 bits resolution, which can not be configured. The LPC55xx has ADC which can be configured as 16 bits resolution or 12 bits resolution.

BR

XiangJun Rong

0 Kudos
Reply