LPC54016JET100 USART3 OUTPUT PROBLEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54016JET100 USART3 OUTPUT PROBLEM

1,981件の閲覧回数
afzhang
Contributor I

In our circuit diagram, PIN0_2 and PIN0_3 are used as serial ports. PIN0_2  and PIN0_3  are configured as USART3.But can not output messages.What should I pay attention to when configuring as usart3.Thanks.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,892件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think you can refer to the following code to configure the pin as uart3:


#define IOCON_PIO_DIGITAL_EN 0x0100u  /*!<@brief Enables digital function */
#define IOCON_PIO_FUNC1 0x01u         /*!<@brief Selects pin function 1 */
#define IOCON_PIO_INPFILT_OFF 0x0200u /*!<@brief Input filter disabled */
#define IOCON_PIO_INV_DI 0x00u        /*!<@brief Input function is not inverted */
#define IOCON_PIO_MODE_INACT 0x00u    /*!<@brief No addition pin function */
#define IOCON_PIO_MODE_PULLUP 0x20u   /*!<@brief Selects pull-up function */
#define IOCON_PIO_OPENDRAIN_DI 0x00u  /*!<@brief Open drain is disabled */
#define IOCON_PIO_SLEW_STANDARD 0x00u /*!<@brief Standard mode, output slew rate control is enabled */

void uart3PinAssignment(void)
{
     uint32_t pin_config;
    //PINs Configuration for Master
      CLOCK_EnableClock(kCLOCK_Iocon);
      CLOCK_EnableClock(kCLOCK_Gpio0);
     // P0_2/FC3_TXD,
    pin_config = (/* Pin is configured as FC3_TXD */
                                         IOCON_PIO_FUNC1 |
                                         /* Selects pull-up function */
                                         IOCON_PIO_MODE_PULLUP |
                                         /* Input function is not inverted */
                                         IOCON_PIO_INV_DI |
                                         /* Enables digital function */
                                         IOCON_PIO_DIGITAL_EN |
                                         /* Input filter disabled */
                                         IOCON_PIO_INPFILT_OFF |
                                         /* Standard mode, output slew rate control is enabled */
                                         IOCON_PIO_SLEW_STANDARD |
                                         /* Open drain is disabled */
                                         IOCON_PIO_OPENDRAIN_DI);

    IOCON_PinMuxSet(IOCON, 0, 2, pin_config);

    // P0_3/FC3_RXD,
    pin_config = (/* Pin is configured as FC3_RXD */
                                           IOCON_PIO_FUNC1 |
                                           /* Selects pull-up function */
                                           IOCON_PIO_MODE_PULLUP |
                                           /* Input function is not inverted */
                                           IOCON_PIO_INV_DI |
                                           /* Enables digital function */
                                           IOCON_PIO_DIGITAL_EN |
                                           /* Input filter disabled */
                                           IOCON_PIO_INPFILT_OFF |
                                           /* Standard mode, output slew rate control is enabled */
                                           IOCON_PIO_SLEW_STANDARD |
                                           /* Open drain is disabled */
                                           IOCON_PIO_OPENDRAIN_DI);
      
     IOCON_PinMuxSet(IOCON, 0, 3, pin_config);

    //Reset FC3
    SYSCON->PRESETCTRL[1]|=1<<14;
    SYSCON->PRESETCTRL[1]&=~(1<<14);
    //set gated clock of FC3
    SYSCON->AHBCLKCTRL[1]|=1<<14;
    //set the FC3 as spi
    FLEXCOMM3->PSELID=0x01;
    //set uart3 clock divider
    //select 12MHz FRO_12M
    SYSCON->FCLKSEL[3]=0x00;

}

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

1,892件の閲覧回数
afzhang
Contributor I

Hi XiangJun Rong:

Thanks!

BR

Aifei Zhang

发件人: xiangjun.rong

发送时间: 2019年12月9日 14:01

收件人: Aifei Zhang

主题: Re: - Re: LPC54016JET100 USART3 OUTPUT PROBLEM

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC54016JET100 USART3 OUTPUT PROBLEM

reply from xiangjun.rong <https://community.nxp.com/people/xiangjun.rong?et=watches.email.thread> in LPC Microcontrollers - View the full discussion <https://community.nxp.com/message/1242844?commentID=1242844&et=watches.email.thread#comment-1242844>

0 件の賞賛
返信