LPC536: Can not enter background mode after changing a register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC536: Can not enter background mode after changing a register

ソリューションへジャンプ
1,635件の閲覧回数
jsoccerd
Contributor II

I'm programming with a custom board that has the LPC536JBD64 processor. The first board I changed the MAINCLKSELA register in the SYSCON peripheral to use the FRO1mhz clock. Then I got a programming error stating that it "Can not enter background mode" with a pemicro multilink. With the pemicro Cyclone programmer I get the error 0007. I then tested a second board with different programs and the programming for that board worked fine. I then tried to recreate the issue by changing the value in the MAINCLKSELA register again and now the same problem has occurred with that board. I'm assuming because I didn't enable bits for that FRO1mhz clock that the board doesn't work. But why would that cause an issue with programming the board over SWD? And is there anyway to unbrick these boards?

0 件の賞賛
返信
1 解決策
1,620件の閲覧回数
jsoccerd
Contributor II

Found a solution on how to unbrick the board. You can use the flashmagic tool and select a processor with a similar enough flash and RAM memory to flash a new program on the board. There is no individual support for the LPC5536.I used the LPC55S66 processor over UART setting. To set the board in ISP mode go to page 909 on the reference manual. To find the UART pins go to page 910 on the reference manual(both in Boot Rom chapter). I am still curious as to why changing the register bricks the SWD programming.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,621件の閲覧回数
jsoccerd
Contributor II

Found a solution on how to unbrick the board. You can use the flashmagic tool and select a processor with a similar enough flash and RAM memory to flash a new program on the board. There is no individual support for the LPC5536.I used the LPC55S66 processor over UART setting. To set the board in ISP mode go to page 909 on the reference manual. To find the UART pins go to page 910 on the reference manual(both in Boot Rom chapter). I am still curious as to why changing the register bricks the SWD programming.

0 件の賞賛
返信