LPC51U68 generate sound

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC51U68 generate sound

1,355件の閲覧回数
larry781111
Contributor I

How can I use LPC51U68 to generate sound? Is there guideline or sample code?

Is it possible to play speech recording file?

0 件の賞賛
返信
1 返信

1,306件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi YuChia Chien,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) How can I use LPC51U68 to generate sound?
-- Yes, as the LPC51U68 has the I2S bus interface.
2) Is there a guideline or sample code?
-- Please refer the application note:
https://www.nxp.com/docs/en/application-note/AN11819.pdf
3) Is it possible to play speech recording file?
-- Of course, the MCU can receive the audio data from the USB, read the audio file in the SD, etc, then, play it via I2S transfer this data to the audio amplifier.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信