LPC51U68 USB Host CDC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC51U68 USB Host CDC

ソリューションへジャンプ
3,008件の閲覧回数
fusheng_huang
Contributor I

Hi all :

I want to implement usb host cdc function on LPC51U68.

But  I didn't found any example code in 51U68 SDK.

anyone could support me about this ?

 

I found usb host cdc example in LPC54608 SDK.

Can I use this example in LPC51U68 ? and anything I need to modify ?

0 件の賞賛
返信
1 解決策
2,996件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi fusheng_huang

LPC51U68 supports USB device interface only. It doesn't support USB host interface.

So there is no USB host example.

ZhangJennie_0-1605234006705.pngZhangJennie_0-1605234006705.png

 

Hope this helps,

Jun Zhang

 

元の投稿で解決策を見る

4 返答(返信)
2,598件の閲覧回数
wsd
Contributor I

Hi,

according to an revision of the data sheet and the user manual the controller has a full speed HOST and device USB controller. Is there any way to implement a host device, otherwise the data sheet is very misleading.

um host device.pngum host device.png

0 件の賞賛
返信
2,997件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi fusheng_huang

LPC51U68 supports USB device interface only. It doesn't support USB host interface.

So there is no USB host example.

ZhangJennie_0-1605234006705.pngZhangJennie_0-1605234006705.png

 

Hope this helps,

Jun Zhang

 

2,990件の閲覧回数
fusheng_huang
Contributor I

because I found USB host folder in SDK, I believe....

anyway, thanks for your reply.

0 件の賞賛
返信
2,985件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信