LPC51U68 RTC Crystal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC51U68 RTC Crystal

跳至解决方案
3,903 次查看
jplathuile
Contributor III

Hi

Concerning a LPC51U68 and the RTC clock.
For using the deep sleep mode, I use the RTC clock, with the crystal I have tried I got weird result. With some crystal a huge jitter, with other an annoying instability the oscillator stall.

The datasheet are not of a great help, it seems on some other nxp device that some capacitor are already included in the chip, but no mention of what to connect.

Can you give me one or two crystal references with the appropriate capacitor, that I can order at Mouser.

Tks

标签 (1)
0 项奖励
回复
1 解答
3,819 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

in DS, there is Cx formula as below. 

pastedImage_2.png

Cx depends on :

CL - Crystal load capacitance, please check your crystal manual for it. 
CPad - Pad capacitance of the RTCXIN and RTCXOUT pins (~3 pF).

CParasitic – Parasitic or stray capacitance of external circuit.

on LPCXpresso51U68 demo board, the Cx is 18pF. Crystal is SSPT7F-12.5pF20-R

see below.

pastedImage_3.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,820 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

in DS, there is Cx formula as below. 

pastedImage_2.png

Cx depends on :

CL - Crystal load capacitance, please check your crystal manual for it. 
CPad - Pad capacitance of the RTCXIN and RTCXOUT pins (~3 pF).

CParasitic – Parasitic or stray capacitance of external circuit.

on LPCXpresso51U68 demo board, the Cx is 18pF. Crystal is SSPT7F-12.5pF20-R

see below.

pastedImage_3.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,819 次查看
jplathuile
Contributor III

Hi,
Thanks for the answer, you have information I don't have, from your site I downloaded,UM11071User manual Rev. 1.2 — 13 August 2019, and there is no mention of the page you gave me.

Ok for the demo board schematic, and I go for that solution.


Regards

JP

0 项奖励
回复
3,819 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

My typo. it's on LPC51U68 datasheet. Thanks for the reminder.

I will revise my original answer *UM* --> "DS"

https://www.nxp.com/docs/en/data-sheet/LPC51U68.pdf 

0 项奖励
回复
3,819 次查看
jplathuile
Contributor III

Hi,

Ok,

with the crystals i tried ( cylindrical case) and different capacitor i can't have a stable oscillation.
I hope on the reference you gave me.

Regards

JP

0 项奖励
回复