LPC43xx debug GPIOs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43xx debug GPIOs

1,301件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jimmcwin on Sun Apr 22 23:21:36 MST 2012
Hi all,

My need is to have two GPIO pins to interface with external module from lpc43xx and I am not any proper signal to mux them in for 2 GPIO pins. I prefer not to use LEDS via I2C interface nor switches. I was hoping for couple reserved pins which can muxed in and configured as GPIO. Have anyone done this similar work on LPC43XX ?

Thanks

Jim
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,285件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PhilYoung on Sun May 13 00:29:09 MST 2012
I think you are looking for LPC_SCU->PINTSEL0 which is defined in the latest version.
0 件の賞賛
返信

1,285件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jimmcwin on Thu May 10 15:13:23 MST 2012
Problem is fixed. However, found one more issue with GPIO codes. The current LPC43XX code does not define LPC_GPIOINT. why ??
0 件の賞賛
返信