LPC43xx Timer Interrupt Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx Timer Interrupt Issue

3,383 Views
samkaos
Contributor I

I have written some pulse control software for LPC4337 @ 200MHz.  Some code is in M0 but of no consequence.  Most of the code is in M4.

M4:-

It uses 4 timers (0-3), and 4 Match compares per timer.  1us timer clock

The Matches generate interrupts, and those interrupts check the IR[] to find the source, clear that bit, and manually control an individual GPIO output.

Something strange is happening.  At random intervals (anywhere from 18 seconds to 20 mins), Timer 2 Match 3 INT gets missed! ALL OTHER TIMER INTS ARE OK.  It will miss a single INT, then next time the compare register is set the INT works fine.  

I cannot explain it, all INTs use similar code, and the code that sets the compare registers is similar.

So, Timer 0 Match 0-3 OK

Timer 1 Match 0-3 OK

Timer 2 Match 0 OK, 1 OK, 2 OK, 3 Glitches (IR[2] & 0x08)

Timer 3 Match 0-3 OK

SCT is unused

-Sam

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

3,102 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I do a quick test with LPCXpresso4337 board Timer2 match 3 at [timers] of [lpcopen_3_02_keil_iar_xpresso4337] software package.

I don't find you mentioned issue.

Could you only do the test with Timer2 Match3, if there still with the same issue?

I attached my test code for your reference.

best regards,

Mike

0 Kudos
Reply

3,102 Views
samkaos
Contributor I

Trigger software (activated by an external trigger)

                                                if (Number == 0 && PipNum == 1)

                                                {

                                                                LPC_GPIO_PORT->SET[3] |= 0x00000020;                                                                                                             LPC_TIMER2->MR[0] = LPC_TIMER2->TC + Want;

                                                                LPC_TIMER2->IR |= 1;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                                else if (Number == 1 && PipNum == 2)

                                                {

                                                                LPC_GPIO_PORT->SET[3] |= 0x00000010;                                                                                                             LPC_TIMER2->MR[1] = LPC_TIMER2->TC + Want;

                                                                LPC_TIMER2->IR |= 2;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                                else if (Number == 2 && PipNum == 3)

                                                {

                                                                LPC_GPIO_PORT->SET[2] |= 0x00000010;                                                                                                             LPC_TIMER2->MR[2] = LPC_TIMER2->TC + Want;

                                                                LPC_TIMER2->IR |= 4;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                                else if (Number == 3 && PipNum == 4)

                                                {

                                                                LPC_GPIO_PORT->SET[5] |= 0x00010000;                                                                                                             LPC_TIMER2->MR[3] = LPC_TIMER2->TC + Want;

                                                                LPC_TIMER2->IR |= 8;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                                else if (Number == 4 && PipNum == 5)

                                                {

                                                                LPC_GPIO_PORT->SET[2] |= 0x00004000;                                                                                                             LPC_TIMER3->MR[0] = LPC_TIMER3->TC + Want;

                                                                LPC_TIMER3->IR |= 1;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                                else if (Number == 5 && PipNum == 6)

                                                {

                                                                LPC_GPIO_PORT->SET[2] |= 0x00000004;                                                                                                             LPC_TIMER3->MR[1] = LPC_TIMER3->TC + Want;

                                                                LPC_TIMER3->IR |= 2;    // Clear Flag

                                                                Number ++;

                                                                if (Number >= 6)

                                                                                Number = 0;

                                                }

                                }

0 Kudos
Reply

3,102 Views
samkaos
Contributor I

Timer INT routines:-

void TIMER2_IRQHandler(void) // Switch off solenoids  1-4

{

                asm("CPSID i"); // Disable all interrupts

                if ((LPC_TIMER2->IR & 0x01) != 0)            

                {

                                LPC_TIMER2->IR |= 1;    // Clear Flag

                                if (oneshot == 1)

                                {

                                                oneshot = 2;

                                                LPC_GPIO_PORT->CLR[3] |= 0x00000010;

                                                LPC_GPIO_PORT->CLR[2] |= 0x00000010;

                                                LPC_GPIO_PORT->CLR[5] |= 0x00010000;

                                                LPC_GPIO_PORT->CLR[2] |= 0x00004000;

                                                LPC_GPIO_PORT->CLR[2] |= 0x00000004;

                                                LPC_GPIO_PORT->CLR[2] |= 0x00000002;

                                                LPC_GPIO_PORT->CLR[2] |= 0x00000001;

                                }

                                LPC_GPIO_PORT->CLR[3] |= 0x00000020;

                }

                if ((LPC_TIMER2->IR & 0x02) != 0)            

                {

                                LPC_TIMER2->IR |= 2;    // Clear Flag

                                LPC_GPIO_PORT->CLR[3] |= 0x00000010;

                }

                if ((LPC_TIMER2->IR & 0x04) != 0)            

                {

                                LPC_TIMER2->IR |= 4;    // Clear Flag

                                LPC_GPIO_PORT->CLR[2] |= 0x00000010;

                }

                if ((LPC_TIMER2->IR & 0x08) != 0)            

                {

                                LPC_TIMER2->IR |= 8;    // Clear Flag

                                LPC_GPIO_PORT->CLR[5] |= 0x00010000;

                }

                LPC_TIMER2->IR |= 0xF0;

                asm("CPSIE i");  // Enable all interrupts

}

//

//

//

void TIMER3_IRQHandler(void)

{

                asm("CPSID i"); // Disable all interrupts

                if ((LPC_TIMER3->IR & 0x01) != 0)            

                {

                                LPC_TIMER3->IR = 1;      // Clear Flag

                                LPC_GPIO_PORT->CLR[2] |= 0x00004000;

                }

                if ((LPC_TIMER3->IR & 0x02) != 0)            

                {

                                LPC_TIMER3->IR = 2;      // Clear Flag

                                LPC_GPIO_PORT->CLR[2] |= 0x00000004;

                }

                if ((LPC_TIMER3->IR & 0x04) != 0)            

                {

                                LPC_TIMER3->IR = 4;      // Clear Flag

                                LPC_GPIO_PORT->CLR[2] |= 0x00000002;

                }

                if ((LPC_TIMER3->IR & 0x08) != 0)            

                {

                                LPC_TIMER3->IR = 8;      // Clear Flag

                                LPC_GPIO_PORT->CLR[2] |= 0x00000001;

                }

 

//            LPC_TIMER3->IR |= 0xF0;

                asm("CPSIE i");  // Enable all interrupts

}

0 Kudos
Reply

3,102 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Sam,

From the description, you are using Timer module for match compares, not State Configurable Timer (SCT).

Could you provide the test code for Timer 2? I could do a onsite test.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply