LPC43xx SDRAM working at high frequencies

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx SDRAM working at high frequencies

756 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by michele_sponchiado_windows on Tue Jun 30 05:59:20 MST 2015
Hi,
I am using the LPC43xx and I've evaluated some boards (WaveShare 4357, EA4357).
In none of these I was able to achieve a SDRAM working frequency bigger than 150MHz.
If I increase the frequency to the next PLL step, I never found a setup where the system works fine, because typically HardFault arise when e.g. using the external memory as a memory pool, or as a heap etc.

I tried changing sfsclk settings as set in AN11508, changing the emc delay clock, using only the CLK1 signal to interface the SDRAM, but without success.

Has anyone every succeded running a SDRAM to frequencies higher than 150MHz?
Thanks
Labels (1)
0 Kudos
Reply
1 Reply

702 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Jun 30 07:11:51 MST 2015
Hi,
150MHz SDRAM frequency is out of specification.The maximum speed is 120MHz. In this case your Core clock should also run at 120MHz.
0 Kudos
Reply