LPC43xx Layout Examples / Reference Design?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx Layout Examples / Reference Design?

3,021 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RandyM on Wed May 08 13:36:13 MST 2013

I see Hitex and Keil have reference hardware for the LPC43xx.  Are the layouts for these designs available for reference?  Are there other layout examples available?


Labels (1)
0 Kudos
Reply
6 Replies

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RandyM on Wed May 15 06:09:14 MST 2013

Thank you for the clarification.

0 Kudos
Reply

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Tue May 14 17:02:00 MST 2013

Hi Randy,


Unfortunately you will have to contact the 3rd party board vendor for board files.


Best regards,


NXP_Support 

0 Kudos
Reply

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RandyM on Tue May 14 08:44:42 MST 2013

Mark,


Agreed!  :-D


0 Kudos
Reply

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mark03 on Mon May 13 10:50:05 MST 2013

Bump.


I think this deserves an answer from an NXP employee.  Even if that answer is "no."


-Mark

0 Kudos
Reply

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RandyM on Wed May 08 14:25:06 MST 2013

Thank you for the schematic links, definitely helpful.  No layout references though?  Do Hitex or Keil make these available upon purchase of their hardware? I'm new to BGA so the fan out and placement of bypass caps is a bit daunting (I see NXP has a <a href="http://www.nxp.com/documents/application_note/AN10778.pdf">generic app note</a>, but a specific example would give extra reassurance when performing the layout).  Browsing through the LPC43xx manual I'm not seeing any layout guidance, even for circuits which are layout critical such as memory and ethernet. 

0 Kudos
Reply

2,912 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed May 08 13:48:30 MST 2013

Hi Randy
The schematics for the Hitex board can be downloaded from:
<a href="http://www.hitex.com/index.php?id=lpc1800-download">http://www.hitex.com/index.php?id=lpc1800-download</a>
The Keil schematics are available at:
<a href="http://www.keil.com/mcb4300/">http://www.keil.com/mcb4300/</a>


0 Kudos
Reply