LPC43xx LPCOpen 2.12 lack of EEPROM example.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43xx LPCOpen 2.12 lack of EEPROM example.

3,272件の閲覧回数
mengxp
Contributor II


Where can I get a EEPROM example?

And Chip_EEPROM_Init -> setWaitState

EEPROM_READ_WAIT_STATE_VAL

EEPROM_WAIT_STATE_VAL

Are these two defines corrected? What core clock running when set these two value?

Now my problem is after Chip_EEPROM_Init(LPC_EEPROM)

Read a DWORD from EEPROM_START will cause a Memory Fault, why?

ラベル(2)
4 返答(返信)

2,600件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

I'd highly recommend you to refer to the EEPROM demo which is from the LPC43xx CMSIS-Compliant Standard Peripheral Firmware Driver Library, please go to LPC43xx CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR) | www.LPCware.com 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,600件の閲覧回数
ahoyhoy
Contributor I

Hi Ping,

Thanks very much for this. Just had a quick read through of this and there should be enough there for me to work from.

Thanks again

0 件の賞賛
返信

2,600件の閲覧回数
ahoyhoy
Contributor I

any luck with this? I am currently trying to implement the internal eeprom on the lpc 4353 and can't see how to set the address you want to write/read data to

0 件の賞賛
返信

2,600件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信