LPC43xx I2S interface with 24bit DAC and ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx I2S interface with 24bit DAC and ADC

1,791 Views
jonathansmith
Contributor III


I am upgrading an existing design to use a LPC43xx processor. The board has a 24bit DAC and a 24bit ADC with I2S interfaces. I was planning to use the I2S interface on the NXP chip, but after re-reading the manual I see that the interface is only capable of handling 8, 16 or 32 bit word sizes.

Any ideas on a solution for interfacing with 24 bit I2S devices?

Many thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,615 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jonathan Smith,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
To achieve your purpose, I think the SGPIO is good choice which is capable of simulating the I2S interface, even customize some features likes support handle 24 bits sizes.
And you can find the example in the 20.8 Examples in the reference manual.
Hope this helps.
Have a great day.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
0 Kudos
Reply