LPC43xx / Gainspan Interaction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx / Gainspan Interaction

2,211 Views
MikeBrennan
NXP Employee
NXP Employee

I've got your LPCXpresso43xx/18xx Vrs 3 Rev B and GainSpan SDIOWAB-GW
Rev 1 card with LPC43S67 checked on the back.  I've downloaded and
activated the LPCXpresso IDE.  I have a TeraTerm virtual terminal running.


I imported projects from LPCOpen->LPC4300 Series, Latest LPCOpen v2.xx tab,
v2.16.  The LPCXpresso toolchain wasn't available but it turned out it was
bundled with the IAR toolchain.

I built and ran the periph_sdio project.  It failed to detect the GainSpan
card.  Terminal displays: "DBG: SDIO Card init error: 0xFFFFFFFE,
-2"


There's a readme in the project that says:
"Example description  This example initializes/enumerates the GainSpan
SDIO card and will enable users to interact with the card using the UART.
Keystrokes captured from UART is submitted to the CARD via SDIO and the
response from the CARD is printed on the UART terminal.

Special connection requirements On the LPC4337 Xpresso shield board JP3 must be
soldered to shunt."

Unfortunately, there's a resistor at J3...   I think I'm stuck unless
there's another example project or board.

 

Any ideas would be appreciated!


Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

1,898 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Michael,

I see that this question has already been addressed on the Case Number 00080289.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply

1,898 Views
omidathari
Contributor II

Hello,

I have thew same issue.

"DBG: SDIO Card init error: 0xFFFFFFFE,-2"

 Where can I find case # related to this issue.

0 Kudos
Reply