LPC43xx Fireware update by IAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx Fireware update by IAP

2,507 Views
skysky
Contributor III

Are there any routines to demonstrate how to upgrade the firmware through the IAP?

LPCOpen has a example - examples\periph\flashiap.

But this routine doesn't solve the problems I'm having right now.

My firmware needs to use the dual BANK address space in lpc4357.

And the firemware file format is BIN,it is read by USB from U-Disk.

So,when i read a section BIN file,i don't know write the program into which flash sector of dual BANK.

In other words, when I write the entire BIN file to flash, the address at compile time in BIN is not corresponding to the address being written.

0 Kudos
Reply
2 Replies

2,247 Views
jeremyzhou
NXP Employee
NXP Employee

Hi sky sky

Please checking the reply in the thread: 求助:LPC4357 IAP应用程序升级方法
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,247 Views
skysky
Contributor III

hi jeremy:

 the thread: 求助:LPC4357 IAP应用程序升级方法 has no reply.

In addtion,"the thread: 求助:LPC4357 IAP应用程序升级方法 " is what i posted

0 Kudos
Reply