LPC43S67 floating point

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43S67 floating point

1,740 Views
john_schooling
Contributor I

Do the LPC4367 and LPC43S67 have M4F (with FPU) or is it just an M4?

Labels (1)
0 Kudos
Reply
2 Replies

1,613 Views
leecoakley
Contributor III

All the optional features are present. It has the FPU, ITM, ETM, MPU, Systick, 6c/2d breakpoints, and I think eight levels of NVIC priority.

Also worth noting that the secondary M0 cores don't have the fast multipliers, but the 32-cycle ones.

1,613 Views
soledad
NXP Employee
NXP Employee

Hi,

The LPC43S67 and LPC4367 contain the ARM Cortex-M4 which is a hardware Floating Point Unit (FPU).


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply