LPC43S67 - dual core app and M0Sub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43S67 - dual core app and M0Sub

1,269件の閲覧回数
christophevarin
Contributor I

Hi,

I'm trying to getting started with the LPC43S67 tripple core (M4 + M0 + M0sub) and make a first app using the M4 and the M0sub.

I'm using Keil usvision to make the code and the OM13084 board from nxp.

My question is, someone already try to program a dual core application and debug it using Keil ? and can you provide some example or hints to start it ?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,072件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the LPCOpen example

https://www.nxp.com/downloads/en/software/lpcopen_3_01_keil_iar_nxp_lpcxpresso_4337.zip 

after download it, you will find some multicore examples in the path:

...lpcopen_3_01_keil_iar_nxp_lpcxpresso_4337\LPC43xx_18xx\examples_43xx_18xx

I hope this helps,

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信