LPC43S37 issue reading E2prom after power-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43S37 issue reading E2prom after power-up

2,213件の閲覧回数
StefanoGattazzo
NXP Employee
NXP Employee

Hi Everyone,

I have a customer using the LPC43S37JET100 that has a problem with internal E2prom.

After Power-on sometimes it is not possible to read the e2prom - the reading value is always 0.

See below the calls related - BSP is LPCOpen 3.02 for LPC43S37. 

 lpc.png

In the manual a time is specified for e2prom reset:

lpcman.jpg

This time is not included in the SW - if the customer is adding a delay the function seems to work fine.

The customer wants to know if we can confirm this is the issue and no others.

BR

Stefano

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,137件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stefano,

I think it is the reason to read incorrect EEPROM data. After power-up, you have to delay some time until the EEPROM initialization is over, then read EEPROM.

Hope it can help you

BR

XiangJun rong

0 件の賞賛
返信

2,137件の閲覧回数
StefanoGattazzo
NXP Employee
NXP Employee

Hi xiangjun.rong ,

In fact, adding a delay, it seems the issue disappears.

The customer wants to have the confirmation this is the issue and not others.

In our SW seems the delay is not inserted.

BR
Stefano

0 件の賞賛
返信

2,137件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,  Stefano,

I think it is the issue. The EEPROM has to be initialized before user can read/write, in other words, user can read/write EEPROM only after the EEPROM initialization is over.

Hope it can help you

BR

XiangJun Rong