LPC4370 errata / bugs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 errata / bugs

3,027件の閲覧回数
inspire
Contributor II

Hi,

The LPC4370 has some bugs that are mentioned in the errata sheet. Is there a plan to fix some of those bugs like it was done for other LPCs? Especially the C_CAN.1 or EMC.1 bugs?

Thank you!

inspire

ラベル(1)
4 返答(返信)

2,681件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Martin,

This problem has been fixed in the flash-based devices (LPC435x/3x/2x/1x), the Rev A of the silicon does not present these bugs:

http://www.nxp.com/documents/errata_sheet/ES_LPC435X_3X_2X_1X_FLASH.pdf 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

2,681件の閲覧回数
inspire
Contributor II

Hi Carlos,

thanks for your response! However, a third core would be very useful for us...besides, do you know if the LPC4370 and the 435x are footprint compatible? 

Thanks!

0 件の賞賛
返信

2,681件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Martin,

 

Unfortunately the flashless devices are currently not scheduled to be fixed. Yes, the parts are footprint compatible.


Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

2,681件の閲覧回数
inspire
Contributor II

alright, thanks a lot, Carlos!

0 件の賞賛
返信