LPC4370 debug error: Unable to connect wire for probe index 1. Error: Wire Ack Fault - target conne

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 debug error: Unable to connect wire for probe index 1. Error: Wire Ack Fault - target conne

2,956件の閲覧回数
chenghaoliu
Contributor I

chenghaoliu_0-1723984689514.pngchenghaoliu_1-1723984721655.pngchenghaoliu_2-1723984745157.png

I 'v already finished Configure LPC4370 in USB device mode, which is :

Completed the basic USB stack configuration and descriptor settings; and set it to Mass Storage Class (MSC). In this way, as then LPC4370 will be recognized as a storage device.

The above part is compiled without any errors.

But once I tried to import the compiled project into the LPC-link 2 board connected to the computer, this error kept appearing:

Unable to connect wire for probe index 1.

Error: Wire Ack Fault - target connected?


This error prevented me from importing the compiled code into the LPC4370 board, preventing me from proceeding to the next step.

Could someone help me,thankyou! 

0 件の賞賛
返信
3 返答(返信)

2,929件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @chenghaoliu 

If LPC4370 on LPC-link2 is your target chip, you need another debugger debug. For example connect another LPC-link2 or J-link.

 

BR

Alice

0 件の賞賛
返信

2,917件の閲覧回数
chenghaoliu
Contributor I

hi

aeac95434756e3f10892d3f6f43ead9.jpg

 

chenghaoliu_0-1724051632401.png

I'v connected with two board now,the right one is the issue board, it's always flashing one it powered. I opened a existing test project, just configured the project no additional code with it. it showa it can't find any probes when i try to debug it.

chenghao

0 件の賞賛
返信

2,860件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @chenghaoliu 

Of the two boards, the left one is debugger, the right one is target board. 

There is connection issue with your boards. Please connect as below:

Alice_Yang_0-1724408254829.jpeg

 

BR

Alice

 

0 件の賞賛
返信