LPC4370 and S25FL256SAGMFI0001 Flash Algorithm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 and S25FL256SAGMFI0001 Flash Algorithm

2,179件の閲覧回数
sujayp
Contributor II

Dear NXP Technical Support Services ,

I am writing in regards the programming of the  the keil ulink pro and i was getting some errors which is as follows:-

 *** Using Compiler 'V5.06 update 1 (build 61)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'Target 1'
".\Objects\Example_42_88.axf" - 0 Error(s), 0 Warning(s).
Build Time Elapsed:  00:00:00
Load "E:\\Microvision_projects\\Objects\\Example_42_88.axf"
No Algorithm found for: 00000000H - 0000114BH
Erase skipped!
Error: Flash Download failed  -  "Cortex-M4"
Flash Load finished at 18:29:19

I think the cortex M4 Device selection requires some configuration for  the  SPIFI  Flash programming algorithm and requires  the configuration using the Settings.

May be I require S25FL256SAGMFI0001 Flash Algorithm drivers which is not found in the Keil MDK.

I am using LPC4370FET256 microcontroller interfaced with the external flash memory SPIFI flash memory S25FL256SAGMFI0001 and will you  please help in this regards.

Regards
Sujay

ラベル(8)
1 返信

1,659件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please try using the SPIFI library. http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/lpc-cortex-m-mcus/lpc1800... 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信