LPC4370 USB HOST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 USB HOST

1,464 Views
371153014
Contributor I

Hi, Buddies.

Now I use LPC 4370 to create a project.

The needs to use the OST module of USB to read and write the U disk

but I haven't found any demo. How can I achieve this function?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,376 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

pls download lpcopen v1.03 from this link.

https://www.nxp.com/downloads/en/libraries/lpcopen_v1.03.zip 

under the folder there is mass storage host demo:

lpcopen_v1.03\lpcopen\applications\lpc18xx_43xx\examples\LPCUSBlib\lpcusblib_MassStorageHost

Hope this helps.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply