LPC4370 - Speed with VCOM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 - Speed with VCOM

1,990 Views
mattiad
Contributor II

Dears,

I'm using USB0 port of my LPC4370 as a virtual com.

In this case, which is the speed of the USB communication?

Full speed or High speed?

Best Regards,

Mattia

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,836 Views
mattiad
Contributor II

Thank you Soledad!

I don't understand another thing: in some evaluation boards there are 33Ohm resistances in D+ and D- lines.

In this schematic

https://www.nxp.com/downloads/en/design-support/LPC4330_Xplorer_schematic_OM13027.pdf 

33Ohm are in the USB1 port and not in USB0 port.

Why in some cases are added and in another cases not?

I suppose that fore a Virtual COM link it's better if they are added.


Best Regards,

Mattia

0 Kudos
Reply

1,836 Views
soledad
NXP Employee
NXP Employee

Hi,

USB0 supports all high-speed, full-speed, and low-speed USB-compliant peripherals.

If you are using the usbd_rom_cdc_vcom LPCOpen example, then is high speed.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply